2025-09-01 10:53 AM
I did not understand the significance of the number 65536 in the below code
pHandle->OvfFreq = (uint16_t)(pHandle->TIMClockFreq / 65536U);
/* Set fixed to 150 ms */
pHandle->HallTimeout = 150U;
/* Compute the prescaler to the closet value of the TimeOut (in mS )*/
pHandle->HALLMaxRatio = (pHandle->HallTimeout * pHandle->OvfFreq) / 1000U ;
/* Align MaxPeriod to a multiple of Overflow.*/
pHandle->MaxPeriod = pHandle->HALLMaxRatio * 65536UL;My main confusion is how the OvfFreq with division of 65536 help the code to reduce the calculations. According to my understanding if TIMClockFreq = 170MHz then the time is T = 1/170Mhz i get overflow after 65535, so if the number of overflows are OverflowCnt then the total time elapsed will be 65535*1/170MHz*OverflowCnt + Input capture timer registers.
Solved! Go to Solution.
2025-09-02 3:18 AM
hello @STuser2 ,
please in each STM32G4 project where you encounter this code ?
for a deeper explanation and detailed understanding of this value, I recommend referring to the STM32G4 Reference Manual.Specifically, you can check the section on Advanced-control timers in the following document:
STM32G4 Series Reference Manual (RM0440)
This section thoroughly explains the timer architecture, including the 16-bit timer counter size (65536 counts), overflow behavior, and related timing calculations.
br
2025-09-02 3:18 AM
hello @STuser2 ,
please in each STM32G4 project where you encounter this code ?
for a deeper explanation and detailed understanding of this value, I recommend referring to the STM32G4 Reference Manual.Specifically, you can check the section on Advanced-control timers in the following document:
STM32G4 Series Reference Manual (RM0440)
This section thoroughly explains the timer architecture, including the 16-bit timer counter size (65536 counts), overflow behavior, and related timing calculations.
br
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.