2022-11-22 12:32 AM
Calling HAL_TIM_OC_Stop_IT causes HAL_TIM_Base_Start_IT to also stop, is this normal? i want to stop a channel, not the entire base timer.
How do i achieve this? re-enabling the base timer after stopping the Channel is not working.
2022-11-22 3:14 PM
It's all the same for HAL_TIM_OC_Stop(), HAL_TIM_OC_Stop_IT(), HAL_TIM_OC_Stop_DMA() functions.
Edited by moderation team to adhere to community guidlines.
2022-12-02 1:56 AM
Hi @BSarn.1 ,
I reported this issue to our development team for deeper analysis. Meanwhile, could you please try to use the LL drivers?
Internal ticket number: 140440(This is an internal tracking number and is not accessible or usable by customers).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-12-02 2:22 AM
i have solved for myself but i had to make a modification into the stm32f4xx_hal_tim.c
on line 1011 i have made:
/* Disable the Peripheral */
//__HAL_TIM_DISABLE(htim); //removed manuallythen the base timer will continue as i desire.
2022-12-03 8:33 AM
Actually it's even worse - just search for all instances of "__HAL_TIM_MOE_DISABLE" in that file and all of those functions are broken the same way. Therefore the affected functions can be described as:
HAL_TIM_***_Stop***()
2022-12-04 6:55 PM
A dirty workaround would be to disconnect the timer signal from ita pin by changin MODE bitfield from 10b
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.