2020-08-19 11:39 PM
Hello,
I have a simple project. I'm using FreeRTOS and programmed TIM2 1ms interrupt.
The TIM2_IRQHandler and PeriodElapsCallback are only called once in the beginning but not after.
I set Clock at 64MHz, the PSC is 63999 and Counter period is 9 I expect 1ms interrupt. I set NVIC TIM2 global intterupt.
I intend to use vTaskNotifyGiveFromISR but first need to make TIM2 interrupt to work.
The real time tasks seem to work fine.
Currently I programmed a counter increment in the PeriodElapsCallback to make sure it works.
I attached the project if someone can support and check. I am probably missing something.
Thanks
2020-08-20 3:47 AM
I'm not sure what I've changed, in any case the PeriodElapseCallback works ok if I have the test increment counter code.
But I'm back in problems if I call vTaskNotifyGiveFromISR. I may not use correct task handler.
In the main.c file I have
extern osThreadId UserTaskIMUHandle;and the call for vTaskNotifyGiveFromISR is
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
/* USER CODE BEGIN Callback 0 */
/* USER CODE END Callback 0 */
if (htim->Instance == TIM1) {
HAL_IncTick();
}
/* USER CODE BEGIN Callback 1 */
if (htim->Instance == TIM2)
{
BaseType_t xHigherPriorityTaskWoken;
xHigherPriorityTaskWoken = pdFALSE;
vTaskNotifyGiveFromISR( UserTaskIMUHandle, &xHigherPriorityTaskWoken );
portYIELD_FROM_ISR( xHigherPriorityTaskWoken );
}In the freertos.c I have
void StartUserTaskIMU(void const * argument)
{
/* USER CODE BEGIN StartUserTaskSND */
uint32_t ulNotifyValue;
for(;;)
{
ulNotifyValue = ulTaskNotifyTake(pdTRUE, 0xFFFFFFFF);
if(ulNotifyValue != 0)
{
// User code
}
}Would someone support to check if this is correct please?
Thanks
2020-08-20 6:34 AM
Some more details that I found ...
The run stops and holds in the Tasks.c file at line "configASSERT( xTaskToNotify )" in the function ...
void vTaskNotifyGiveFromISR( TaskHandle_t xTaskToNotify, BaseType_t *pxHigherPriorityTaskWoken )Should I suspect it is something about the task handler?
2020-08-20 6:52 AM
Double check that the tasks are created (and the assigned handle is not NULL) before arming the interrupt.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.