2020-03-23 1:14 AM
Version:
#define __STM32L0xx_HAL_VERSION_MAIN (0x01U) /*!< [31:24] main version */
#define __STM32L0xx_HAL_VERSION_SUB1 (0x0AU) /*!< [23:16] sub1 version */
#define __STM32L0xx_HAL_VERSION_SUB2 (0x02U) /*!< [15:8] sub2 version */
#define __STM32L0xx_HAL_VERSION_RC (0x00U) /*!< [7:0] release candidate */
File Drivers\STM32L0xx_HAL_Driver\Inc\stm32l0xx_hal_tim.h
static void TIM_CCxChannelCmd(TIM_TypeDef *TIMx, uint32_t Channel, uint32_t ChannelState)
{
uint32_t tmp;
/* Check the parameters */
assert_param(IS_TIM_CC1_INSTANCE(TIMx));
assert_param(IS_TIM_CHANNELS(Channel));
tmp = TIM_CCER_CC1E << (Channel & 0x1FU); /* 0x1FU = 31 bits max shift */
/* Reset the CCxE Bit */
TIMx->CCER &= ~tmp;
/* Set or reset the CCxE Bit */
TIMx->CCER |= (uint32_t)(ChannelState << (Channel & 0x1FU)); /* 0x1FU = 31 bits max shift */
}
This function assumes CCER has 1 bit per timer, but on this MCU, each timer has 4 bits. Function should have this layout instead:
static void TIM_CCxChannelCmd(TIM_TypeDef *TIMx, uint32_t Channel, uint32_t ChannelState)
{
uint32_t tmp;
/* Check the parameters */
assert_param(IS_TIM_CC1_INSTANCE(TIMx));
assert_param(IS_TIM_CHANNELS(Channel));
tmp = TIM_CCER_CC1E << (Channel & 0x03U)*3;
/* Reset the CCxE Bit */
TIMx->CCER &= ~tmp;
/* Set or reset the CCxE Bit */
TIMx->CCER |= (uint32_t)(ChannelState << (Channel & 0x03U)*3);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.