2022-02-17 2:09 AM
#include "main.h"
/* Private define ------------------------------------------------------------*/
#define FLASH_USER_START_ADDR ADDR_FLASH_PAGE_16 /* Start @ of user Flash area */
#define FLASH_USER_END_ADDR ADDR_FLASH_PAGE_255 + FLASH_PAGE_SIZE - 1 /* End @ of user Flash area */
#define DATA_64 'A'
#define DATA_32 ((uint32_t)0x12345678)
/* Private variables ---------------------------------------------------------*/
uint32_t FirstPage = 0, NbOfPages = 0, BankNumber = 0;
uint32_t Address = 0, PAGEError = 0;
__IO uint32_t data32 = 0 , MemoryProgramStatus = 0;
uint8_t buff[10] = {255,80,9,7,1,2,3,4,5,6};
uint8_t flag;
uint8_t data[10];
/* Private function prototypes -----------------------------------------------*/
static void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_UART_Init(void);
/* Private functions ---------------------------------------------------------*/
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
HAL_UART_Receive_IT(&huart2, data, sizeof(data));
flag = 1;
}
/**
* @brief Main program
* @param None
* @retval None
*/
int main(void)
{
HAL_Init();
/* Configure the system clock to 120 MHz */
SystemClock_Config();
MX_GPIO_Init();
MX_USART2_UART_Init();
HAL_FLASH_Unlock();
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);
Address = FLASH_USER_START_ADDR;
while (1)
{
HAL_UART_Receive_IT(&huart2, data, sizeof(data));
if(flag == 1)
{
HAL_UART_Transmit_IT(&huart2, data, sizeof(data));
while (Address < ADDR_FLASH_PAGE_19)
{
for(uint8_t i = 0; i<10 ;i++)
{
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, Address, data[i]) == HAL_OK)
{
Address = Address + 8;
}
else
{
HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_7);
}
}
}
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_7, GPIO_PIN_SET);
flag = 0;
}
}
HAL_FLASH_Lock();
while (1)
{
}
}
/**
* @brief System Clock Configuration
* The system Clock is configured as follows :
* System Clock source = PLL (MSI)
* SYSCLK(Hz) = 120000000
* HCLK(Hz) = 120000000
* AHB Prescaler = 1
* APB1 Prescaler = 1
* APB2 Prescaler = 1
* MSI Frequency(Hz) = 4000000
* PLL_M = 1
* PLL_N = 60
* PLL_Q = 2
* PLL_R = 2
* PLL_P = 7
* Flash Latency(WS) = 5
* @param None
* @retval None
*/
void SystemClock_Config(void)
{
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
/* Enable voltage range 1 boost mode for frequency above 80 Mhz */
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1_BOOST);
__HAL_RCC_PWR_CLK_DISABLE();
/* Enable MSI Oscillator and activate PLL with MSI as source */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;
RCC_OscInitStruct.MSIState = RCC_MSI_ON;
RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;
RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6;
RCC_OscInitStruct.PLL.PLLM = 1;
RCC_OscInitStruct.PLL.PLLN = 60;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLP = 7;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
/* Initialization Error */
while(1);
}
/* To avoid undershoot due to maximum frequency, select PLL as system clock source */
/* with AHB prescaler divider 2 as first step */
RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if(HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{
/* Initialization Error */
while(1);
}
/* AHB prescaler divider at 1 as second step */
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
if(HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
{
/* Initialization Error */
while(1);
}
}
/**
* @brief USART2 Initialization Function
* @param None
* @retval None
*/
static void MX_USART2_UART_Init(void)
{
huart2.Instance = USART2;
huart2.Init.BaudRate = 115200;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart2.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetTxFifoThreshold(&huart2, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetRxFifoThreshold(&huart2, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_DisableFifoMode(&huart2) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_7, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_14, GPIO_PIN_RESET);
/*Configure GPIO pin : PB7 */
GPIO_InitStruct.Pin = GPIO_PIN_7|GPIO_PIN_14;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
}
#ifdef USE_FULL_ASSERT
void assert_failed(uint8_t *file, uint32_t line)
{
while (1)
{
}
}
#endif
void Error_Handler(void)
{
__disable_irq();
while (1)
{
}
}
2022-02-17 2:25 AM
A comment on you code: Using HAL_UART_Receive_IT, setting a flag in the HAL_UART_RxCpltCallback, and polling for it makes not much sense. And, I think you are polling it wrong.
Why not using polling here directly (HAL_UART_Receive). And, if you insist using a flag, make it volatile.
Don't know about docklight though. Usually there are protocols like xmodem, ymodem, zmodem used for that.
hth
KnarfB
2022-02-17 2:33 AM
Hi @KnarfB, actually my problem is I need to flash application bin file to flash memory using UART bootloader,
So If I want to use STMCube programmer, what i need to configure in bootloader project for the UART configuration...if u know anything about how to do this please let me know...
2022-02-17 6:42 AM
If you want to use STM32CubeProgrammer, you would jump to the ROM bootloader in your code and let it handle things. I agree that using polling would make things easier here, since that's all your application is doing. There are examples on how to write flash in the CubeMX repository. Get the basics working first, then add in the UART handling.
2022-02-17 6:43 AM
Duplicate:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.