2020-07-06 4:48 AM
tcpip thread message fetch is not running in lwIP if caches enabled in STM32F767.
/* Enable I-Cache---------------------------------------------------------*/
SCB_EnableICache();
/* Enable D-Cache---------------------------------------------------------*/
SCB_EnableDCache();
2020-07-06 5:52 AM
Cache management is nontrivial. You can either disable it, or learn how to handle it properly.
https://community.st.com/s/article/FAQ-DMA-is-not-working-on-STM32H7-devices
2020-07-06 2:14 PM
2020-07-13 5:22 AM
Can i get the working example code with lwip.
I feel the problem is lwIP driver Rx data buffers not aligned to cache line size. The address and size of buffers, on which D-cache invalidation are used, must be aligned to __SCB_DCACHE_LINE_SIZE, which is 32 bytes for Cortex-M7.
So expecting properly aligned buffers example code for STM32F767 with lwip for the reference.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.