2017-03-28 7:18 PM
Everybody,
I want to switch between thread on RTOS, how can I do that ?
I've written down below, but it seems that it's staying on the first thread only,
Thanks
/* StartDefaultTask function */
void StartDefaultTask(void const * argument){
/* init code for FATFS */MX_FATFS_Init();
/* init code for USB_DEVICE */
MX_USB_DEVICE_Init();/* USER CODE BEGIN StartDefaultTask */
/* Infinite loop */ test_fatfs(); reading_file_test(); /* Suspend Thread 1 */ osThreadSuspend(NULL); /* Resume Thread 2*/ osThreadResume(secondTaskHandle); /* for(;;) { osDelay(1); } */ /* USER CODE END StartDefaultTask */}void StartSecondTask(void const * argument)
{ reading_file_test(); /* Resume Thread 1 */ osThreadResume(defaultTaskHandle);/* Suspend Thread 2 */
osThreadSuspend(NULL);}#switch #rtos #thread2017-03-30 8:20 PM
I fail to see the need for two threads given the flow chart provided. With that said, do you know how to use a mutex and osThreadYield? The other key piece is that both threads need to have the same priority.
Edit: spelling
2017-03-30 8:28 PM
I don't know on how to use Mutex,
The core is, I want to learn to use FreeRTOS from the scratch,
and I don't know how to use osThreadYield.
Is it possible if we don't have to use Mutex ? or it's a must ? I want
to learn from the simplest step first.
How can I make those two threads have the same priority ?
I follow the example from STM3210C Eval RTOS project,
it seems that I missed something from it, and it's stopped working only
at the first thread and never goes into the 2nd thread.
Could it be, I missed something inside configuration ?
my current attempt :
=========================================
void MX_FREERTOS_Init(void) {
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* USER CODE BEGIN RTOS_MUTEX */
/* add mutexes, ... */
/* USER CODE END RTOS_MUTEX */
/* USER CODE BEGIN RTOS_SEMAPHORES */
/* add semaphores, ... */
/* USER CODE END RTOS_SEMAPHORES */
/* USER CODE BEGIN RTOS_TIMERS */
/* start timers, add new ones, ... */
/* USER CODE END RTOS_TIMERS */
/* Create the thread(s) */
/* definition and creation of defaultTask */
osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 512);
defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL);
/* USER CODE BEGIN RTOS_THREADS */
/* add threads, ... */
/* definition and creation of defaultTask */
osThreadDef(secondTask, StartSecondTask, osPriorityNormal, 0, 512);
secondTaskHandle = osThreadCreate(osThread(secondTask), NULL);
/* USER CODE END RTOS_THREADS */
/* USER CODE BEGIN RTOS_QUEUES */
/* add queues, ... */
/* USER CODE END RTOS_QUEUES */
}
/* StartDefaultTask function */
static void StartDefaultTask(void const * argument)
{
uint32_t count = 0;
(void) argument;
/* init code for FATFS */
MX_FATFS_Init();
/* init code for USB_DEVICE */
MX_USB_DEVICE_Init();
/* USER CODE BEGIN StartDefaultTask */
/* Infinite loop */
printf('Start Default Task! \n');
for (;;)
{//thread1 endless loop begin
test_fatfs(); //task thread_2 1
reading_file_test(); //task thread_2 2
printf('Line 242 <<== \n'); //<=======stops here and
stops forever*
/* Suspend Thread 1 */
osThreadSuspend(NULL);
osDelay(1000);
/* Resume Thread 2*/
osThreadResume(secondTaskHandle);
}//thread1 endless loop end
/*
for(;;)
{
osDelay(1);
}
*/
/* USER CODE END StartDefaultTask */
}
static void StartSecondTask(void const * argument)
{
printf('Start Second Task! \n');
for (;;)
{//thread2 endless loop begin
reading_file_test(); //task on thread 2
/* Resume Thread 1 */
osThreadResume(defaultTaskHandle);
osDelay(1000);
/* Suspend Thread 2 */
osThreadSuspend(NULL);
}//thread2 endless loop end
}
================================
2017-03-30 9:08 PM
Is it possible if we don't have to use Mutex ? or it's a must ? I want
to learn from the simplest step first.
Yes, to make this work reliably, you need to understand how to use some sort of proper thread synchronization primitives.
I don't know that this is the right place to try to learn multi-threaded programming. Take a look at mbed.org. The same CMSIS-OS facilities are available through those tools. They are quite a bit easier to use, and it is more geared towards teaching these sort of concepts by providing a simpler coding model and lots of example code. I use mbed.org to mock up new code all the time -- especially when I'm playing with new hardware.
Until you master these skills, writing a working embedded RTOS application that uses USB is going to be difficult.
2017-03-30 9:29 PM
Thanks for your suggestion for mbed.org.
I'm not going to use USB yet, I will learn on RTOS first, is there a
community for mbed.org ? a place to learn or it's only from the book and
example provided?
I can see the example from STM3210C-EVAL, that's the simplest I can
understand, blink the LED, I want to enter from that starting point (
two threads )
at this point I don't understand yet for 'thread syncronization', on my
mind, turn on one thread and turn off the other one and loop it..
What's API for 'thread RUNNING', 'thread READY','thread WAITING','thread
INACTIVE',
I got osThreadSuspend(NULL); ==> stop the thread
osThreadResume(LEDThread2Handle); ==> start the thread
So I call thread 2 after thread 1 is finished, and thread 2 is doing the
job, ==>finish it's calling thread 1 and I want them in endless loop,
it sounds like I'm doing on while(){} but inside FreeRTOS..
________________ Attachments : gpdglcdfbdgonfff.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hyj6&d=%2Fa%2F0X0000000bBb%2Fh4utBHWVRGEYZFgdIvO5smrdgzw0kSme83gYI.zyPb0&asPdf=false2017-03-30 9:53 PM
I've seen Mbed.org, but I'm not yet in that level, I want to learn
something simple from STM32CubeMX and FreeRTOS, and not making it more
complicated.
Thanks for that.
2017-03-30 10:02 PM
Start here:
https://developer.mbed.org/forum/
It is a great place to learn this stuff.
2017-03-30 10:09 PM
Using mbed.org for development is a lot simpler than using STM32CubeMX. Orders of magnitude simpler. STM32CubeMX exposes a lot of complexity to the developer that is hidden from you in mbed.org.
mbed.org, especially with its online compiler, is designed to be a learning tool, much like the Arduino development environment.
2017-03-30 10:13 PM
Really, I have no idea about that, I'm in the middle of STM32CubeMX now,
it is another task for me switching from STM32CubeMX to Mbed, I reckon.
2017-03-30 10:22 PM
I think, I'll follow : http://www.freertos.org/, there are some books
there...
Thanks for mbed.org suggestions anyway..
2017-03-30 11:51 PM
I learn from FreeRTOS book, the basic of task, but I don't know if I
have missing configuration on my STM32CubeMX, any advice ? thanks
========================================
/3.2 Task Functions//
//Tasks are implemented as C functions. The only thing special about
them is their prototype,//
//which must return void and take a void pointer parameter. The
prototype is demonstrated by//
//Listing 11.//
//void ATaskFunction( void *pvParameters );//
//Listing 11. The task function prototype//
//Each task is a small program in its own right. It has an entry point,
will normally run forever//
//within an infinite loop, and will not exit. The structure of a typical
task is shown in Listing 12.//
//FreeRTOS tasks must not be allowed to return from their implementing
function in any way�?//
//they must not contain a ‘return’ statement and must not be allowed to
execute past the end of//
//the function. If a task is no longer required, it should instead be
explicitly deleted. This is also//
//demonstrated in Listing 12.//
//A single task function definition can be used to create any number of
tasks�?each created task//
//being a separate execution instance, with its own stack and its own
copy of any automatic//
//(stack) variables defined within the task itself.//
//void ATaskFunction( void *pvParameters )//
//{//
///* Variables can be declared just as per a normal function. Each
instance of a task//
//created using this example function will have its own copy of the
lVariableExample//
//variable. This would not be true if the variable was declared static –
in which case//
//only one copy of the variable would exist, and this copy would be
shared by each//
//created instance of the task. (The prefixes added to variable names
are described in//
//section 1.5, Data Types and Coding Style Guide.) *///
//int32_t lVariableExample = 0;//
///* A task will normally be implemented as an infinite loop. *///
//for( ;; )//
//{//
///* The code to implement the task functionality will go here. *///
//}//
///* Should the task implementation ever break out of the above loop,
then the task//
//must be deleted before reaching the end of its implementing function.
The NULL//
//parameter passed to the vTaskDelete() API function indicates that the
task to be//
//deleted is the calling (this) task. The convention used to name API
functions is//
//described in section 1.5, Data Types and Coding Style Guide. ///
/*/vTaskDelete( NULL );//====> osThreadSuspend(NULL); in*STM32CubeMX
API*
//}
=========
/
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.