2015-06-04 5:39 AM
Hi everyone,
I am trying to learn the CMSIS-RTOS RTX. I have experience in FreeRTOS. I am trying to test this example: https://www.keil.com/pack/doc/CMSIS/RTX/html/_example_r_t_x__tutorial.html&sharpRTX_Tutorial_SVCBut my hardware is a STM32F107VC. it's not aSTM32F429. the test program compiles fine but I can't get the test program work fine: This is my code, Iam using the pin PC13 as interrupt line:
/*----------------------------------------------------------------------------
CMSIS-RTOS 'main' function template
*---------------------------------------------------------------------------*/
&sharpdefine osObjectsPublic // define objects in main module
&sharpinclude ''osObjects.h'' // RTOS object definitions
&sharpinclude ''stm32f10x.h''
&sharpinclude ''led_open107v.h''
//&sharpinclude ''joystick_open107v.h''
void led_Thread1(void const *argument);
void led_Thread2(void const *argument);
void exti_Thread(void const *argument);
void __svc(1) init_EXTI(void); //Define the EXTI initializing code as a supervisor function
void UserKey_Configuration(void);
void configInterrupt(void);
osThreadDef(led_Thread1, osPriorityNormal, 1, 0);
osThreadDef(led_Thread2, osPriorityNormal, 1, 0);
osThreadDef(exti_Thread, osPriorityAboveNormal, 1, 0);
osThreadId T_led_ID1;
osThreadId T_led_ID2;
osThreadId T_exti_ID;
void exti_Thread(void const *argument) {
for (;;) {
osSignalWait(0x01, osWaitForever);
LED_On(1);
osDelay(500);
LED_Off(1);
}
}
void led_Thread1(void const *argument) {
for (;;) {
osSignalWait(0x01, osWaitForever);
LED_Off(0);
}
}
void led_Thread2(void const *argument) {
for (;;) {
LED_On(0);
osDelay(500);
osSignalSet(T_led_ID1, 0x01);
osDelay(500);
}
}
/*
main: initialize and start the system
*/
int main(void) {
osKernelInitialize();
init_EXTI(); //initialize the external interrupts
LED_Initialize();
T_led_ID1 = osThreadCreate(osThread(led_Thread1), NULL);
T_led_ID2 = osThreadCreate(osThread(led_Thread2), NULL);
T_exti_ID = osThreadCreate(osThread(exti_Thread), NULL);
osKernelStart(); // start thread execution
}
void __svc(1) init_EXTI (void);
void __SVC_1(void) {
UserKey_Configuration();
configInterrupt();
}
/*----------------------------------------------------------------------------
EXTI interrupt handler
*---------------------------------------------------------------------------*/
void EXTI15_10_IRQHandler(void) {
/* Check if EXTI_Line13 is asserted */
if(EXTI_GetITStatus(EXTI_Line13) != RESET) {
/* [EXTI15_10_IRQHandler] EXTI_Line13 is asserted. KeyUser PC13 */
/* We need to clear line pending bit manually */
osSignalSet(T_exti_ID, 0x01);
EXTI_ClearITPendingBit(EXTI_Line13);
}
}
void UserKey_Configuration(void) {
GPIO_InitTypeDef GPIO_InitStructure;
/* GPIOC Port Clock Enable */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE);
/* User key PC13*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU;
GPIO_Init(GPIOC, &GPIO_InitStructure);
}
void configInterrupt(void) {
EXTI_InitTypeDef EXTI_InitStructure; /* EXTI structure to init EXTI */
NVIC_InitTypeDef NVIC_InitStructure; /* NVIC structure to init NVIC Controller */
/* keyUser PC13 */
GPIO_EXTILineConfig(GPIO_PortSourceGPIOC, GPIO_PinSource13); /* Connect EXTI line to button. Port C and pin 13 */
EXTI_InitStructure.EXTI_Line = EXTI_Line13; /* Configure Button port C and pin 13, EXTI line */
EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; /* Select interrupt mode */
EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Falling; /* Generate interrupt on rising edge */
EXTI_InitStructure.EXTI_LineCmd = ENABLE; /* Enable EXTI line */
EXTI_Init(&EXTI_InitStructure); /* Send values to registers */
/* Configure NVIC */
NVIC_InitStructure.NVIC_IRQChannel = EXTI15_10_IRQn; /* Select NVIC channel to configure */
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x0F; /* Set priority to lowest */
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x0F; /* Set subpriority to lowest */
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; /* Enable IRQ channel */
NVIC_Init(&NVIC_InitStructure); /* Update NVIC registers */
/* End keyuser PC13 */
}
What can I be doing wrong?
Thank you so much, Best regards.
#stm32f1xx #svc #cmsis-rtosWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.