2023-09-27 1:01 AM
Using STM32L451CET6 and threadx I created multiple task and was running into hard fault on debugging found that from my 70KB byte pool when i created a task more than 27Kb it was running into hard fault again the usable memory is 160Kb out of which a partition exists between sram 1 and sram 2 which is of 128kb sram1 and rest sram2 Can anyone suggest why this is happening
Tried changing stack size of tasks, whenever they are under 27/28Kb they work perfectly. but when it is exceeding that limit,it runs into hardfault
2023-09-27 8:27 AM
Your task STACKS are over 27K bytes (or words)? How many tasks do you have? Disclaimer: I have only a little experience with AzureRTOS. There should be some error function when its memory allocator runs out of memory. If so, is that getting called?
2023-10-26 6:34 AM
Hi @Hjain.1 ,
Hope your are doing well.
do you still have the problem?, if it is the case would you please share a project reproducing the issue?
regards
haithem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.