2014-10-27 10:58 PM
Hello,
I have some problems to initialise the Low power timer correctly. I'm using the STM32Cube firmware and a STM32L053R8 chip. To start with the LPTIM, I will only toggle a GPIO but I'll never enter the interrupt handler of the LPTIM.Probably someone has any ideas what's wrong with my code...int main(){ HAL_Init(); __GPIOA_CLK_ENABLE(); GPIO_InitTypeDef gpioOutputStructure1; gpioOutputStructure1.Pin = GPIO_PIN_8; gpioOutputStructure1.Mode = GPIO_MODE_OUTPUT_PP; gpioOutputStructure1.Pull = GPIO_PULLDOWN; gpioOutputStructure1.Speed = GPIO_SPEED_FAST; HAL_GPIO_Init( GPIOA, &gpioOutputStructure1 ); HAL_GPIO_WritePin( GPIOA, GPIO_PIN_8, GPIO_PIN_SET ); initLPTIM(); while( 1 );}void initLPTIM( void ){ uint32_t lptimTicks = 327; /* Enable External Low Speed Clock (LSE) */ RCC_OscInitTypeDef RCC_OscInitStructure; RCC_OscInitStructure.OscillatorType = RCC_OSCILLATORTYPE_LSE; RCC_OscInitStructure.LSEState = RCC_LSE_ON; HAL_RCC_OscConfig( &RCC_OscInitStructure ); /* Select the LSE clock as LPTIM peripheral clock */ RCC_PeriphCLKInitTypeDef RCC_PeriphCLKInitStructure; RCC_PeriphCLKInitStructure.PeriphClockSelection = RCC_PERIPHCLK_LPTIM1; RCC_PeriphCLKInitStructure.LptimClockSelection = RCC_LPTIM1CLKSOURCE_LSE; HAL_RCCEx_PeriphCLKConfig( &RCC_PeriphCLKInitStructure ); /* Initialise LPTIM peripheral */ LPTIM_InitStructure.Init.Clock.Source = LPTIM_CLOCKSOURCE_APBCLOCK_LPOSC; LPTIM_InitStructure.Init.Clock.Prescaler = LPTIM_PRESCALER_DIV1; LPTIM_InitStructure.Init.CounterSource = LPTIM_COUNTERSOURCE_INTERNAL; LPTIM_InitStructure.Init.Trigger.Source = LPTIM_TRIGSOURCE_SOFTWARE; LPTIM_InitStructure.Init.OutputPolarity = LPTIM_OUTPUTPOLARITY_HIGH; LPTIM_InitStructure.Init.UpdateMode = LPTIM_UPDATE_IMMEDIATE; /* Initialise LPTIM peripheral according to the passed paramters */ if( HAL_LPTIM_Init( &LPTIM_InitStructure ) != HAL_OK ) { while( 1 ); } /* Start the Timeout function in interrupt mode */ if( HAL_LPTIM_COUNTER_Start_IT( &LPTIM_InitStructure, 99, 49 ) != HAL_OK ) { while( 1 ); }}void LPTIM1_IRQHandler(void){ /* Autoreload match interrupt */ if( __HAL_LPTIM_GET_FLAG( &LPTIM_InitStructure, LPTIM_FLAG_ARRM ) != RESET ) { if( __HAL_LPTIM_GET_ITSTATUS( &LPTIM_InitStructure, LPTIM_IT_ARRM ) != RESET ) { /* Clear Autoreload match flag */ __HAL_LPTIM_CLEAR_FLAG( &LPTIM_InitStructure, LPTIM_FLAG_ARRM ); HAL_GPIO_TogglePin( GPIOA, GPIO_PIN_8 ); //timer.interruptServiceMethod(); } }} #lptim #stm32cube-stm32l0xxWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.