2016-04-15 4:45 AM
Fellows
on some STM32L0 (STM32L011x3/4 TSSOP2) Boot0 is also PB9 on others (STM32L031x4/6 TSSOP2) only Boot0. Is this not allways the same for a STM32 familiy like STM32L0x? Is that correct? I think on we need as much as possible Pins on the small cases. Therefore it should be a must to havae also a second function on the Boot0 pin. Cheers Felix #stm32l0 #boot02016-04-15 10:00 AM
Well I suspect that would just complicate testing and recovery.
If is possible to have small packages with higher pin counts.2016-04-15 11:55 AM
Hi bonjour.felix,
This is due to the package size which is small. For example, You can find in STM32F4xx devices that boot1 is shared with PB2. -Hannibal-2016-04-15 12:16 PM
No, I think the question being asked is why can't BOOT[0] be a GPIO pin too
2016-04-16 2:15 AM
The first chips were ''many pin'' packages, so it was not necessary to be really careful with the number of pins. Later, smaller packages were added and you see that as time progresses you get more and more options to use the ''special'' pins as GPIOs too if you know what you're doing.
However, Suppose your application uses the SWD pins, and you've set the option register to ''boot from flash''. So now you've got trouble if you need to update the firmware. If your design is good there will still be a way, but without the option of the boot mode, things are even more restricted. I understand that it ''feels'' wrong to have to get a 32 pin package when a 20pin will ALLMOST fit.2016-04-16 2:43 AM
I am not happy with your answer...
TSSOP20: STM32L011x3/4 has PIN1 BOOT0 / PB9 (DocID027973 Rev 3 35/114) TSSOP20: STM32L041x4/6 has PIN1 BOOT0 (DocID027301 Rev 3 36/112) So, same package size (TSSOP20), same family (STM32L0) but differenrt implementaition. Why? Or is one of the data sheet not correct? Regards Felix2016-04-16 2:47 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.