2019-03-13 6:42 AM
I am using an STM32L010k8 device, every second word write to Flash using the HAL driver function HAL_FLASH_Program() generates a write protection fault (WRPERR bit in FLASH_SR). If I retry the write to the same address the error is not present
Is this an errata on the device or bug in the HAL driver? Errata sheet is not available for this device.
2019-03-14 2:34 AM
Hello,
The Errata sheet doesn’t exist now. This is planning in future to write errata for this device.
This is 64kB device, so you can check another STM32L0 errata according the Flash memory as the errata: STM32L053x6 STM32L053x8.
Otherwise, could you please provide more details on the faced issue and which Cube firmware package using ?
Kind Regards,
Imen
2019-03-17 11:47 PM
Hi Imen,
Thanks for the reply. The problem I had turned out to be a corrupt pointer in my application, that was modifying the Flash registers, my apologies for that.
The current version of the HAL flash driver does not support half-page writes, do you know when that will be implemented?
Lastly I have noticed the flash is cleared to zeros when it is erased (and not 0xFFFFFFFF), is this because of the EEPROM/NVM interface?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.