cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7S78-DK

Guyc
Associate

Hello Everyone,

I recently purchased STM32H7S78-DK.
I'm looking for the code that runs on the discovery kit.
As I understood from my collogue there should be an application that defines all the peripherals via cubeMX.
I've downloaded the repository for this DK but all I see is examples that covers some of the peripherals and not one application that defines all the peripherals. 

I would if someone can share with the link for this application that define all the peripherals. 

2 REPLIES 2
NesrynELMK
ST Employee

Hello @Guyc 

 

There is no official reference project that initializes all peripherals for the STM32H7S78-DK. The recommended approach is to use STM32CubeMX to configure the peripherals you need for your specific application, or to use the provided peripheral-specific examples provided in the STM32CubeH7RS package.

 

Br,

Thanks for your answer. let me be more specific.
I'm new to with some of the peripherals I need to configure, for example XSPI, LTDC, FMC etc.
When I look on the examples sometimes I need to combine both examples for my need. 
When I got the DK there was a FW that already burned on it. This the FW I'm looking for, so I'll be to see how it configured on Cube MX.

Thanks in advance. 


Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.