2019-06-11 11:40 PM
Hope all is going well. I'm trying to ping STM32H743ZI NUCLEO 144 using LWIP middle-ware. Code generated by CubeMX.
while(1)
{
MX_LWIP_Process();
}I don't know how should I configure the CubeMX or change the generated code to be able to ping my board.
2019-06-14 4:03 AM
I'm trying for two months and still not able to ping my board.
... Any supports for STM32H743ZI Nucleo 144 board?
2020-05-23 2:20 AM
same face this problem in my stm32h743zi neculo board. if have any code for Ethernet UDP example please share us
2020-05-23 3:23 AM
I was able to successfully awake LwIP on H747ZI and on F4 (on F4, CubeMX generated code worked), but not the one which is in CubeMX. A freshly generated project immendiately throws an ethernet DMA error on H7.
Finally I found an example in CubeMX package, located in: STM32Cube\Repository\STM32Cube_FW_H7_V1.4.0\Projects\NUCLEO-H743ZI\Applications\LwIP\LwIP_HTTP_Server_Netconn_RTOS and it works. Compiled with Atollic true studio (open SW4STM32\STM32H743ZI_Nucleo) and it will compile.
Try to use this example as starting point.
A very simple UDP echo example is here:
struct netbuf *buf;
static void udp_thread(void *arg)
{
struct netconn *conn;
err_t err;
char buffer[256];
/* Create a new TCP connection handle */
conn = netconn_new(NETCONN_UDP);
netconn_bind(conn, IP_ADDR_ANY, 1234);
while (1)
{
err = netconn_recv(conn, &buf);
if (err == ERR_OK)
{
/* no need netconn_connect here, since the netbuf contains the address */
netbuf_copy(buf, buffer, sizeof(buffer));
err = netconn_send(conn, buf);
netbuf_delete(buf);
}
}
}
sys_thread_new("UDP2TH", udp_thread, NULL, 2048, 4);
2020-05-23 10:37 PM
Thanks for reply.
i not use RTOS. i seen stl32h743Zi example but it code is rtos based and also no any found code on UDP based
i also generated using Mx cube but it does not work.
1. i faces some warning "The ETH can work only when RAM is
pointing at 0x24000000"
I was searching but did not find how to solve that.
2. I wrote code for ping command reply but it is not worked
GPIO pin mapping
PA1 ETH_REF_CLK
PA2 ETH_MDIO
PA7 ETH_CRS_DV
PB13 ETH_TXD1
PC1 ETH_MDC n/a
PC4 ETH_RXD0
PC5 ETH_RXD1
PG11 ETH_TX_EN
PG13 ETH_TXD0
Enable
ICMP option
code
while (1)
{
/* USER CODE END WHILE */
MX_LWIP_Process();
/* USER CODE BEGIN 3 */
}
so i required UDP based example on STM32h743zi series.
if have you so please provide us
Reguard's
Hiren
2020-05-25 8:46 PM
Thanks for reply.
i not use RTOS. i seen stl32h743Zi example but it code is rtos based and also no any found code on UDP based
i also generated using Mx cube but it does not work.
1. i faces some warning "The ETH can work only when RAM is
pointing at 0x24000000"
I was searching but did not find how to solve that.
2. I wrote code for ping command reply but it is not worked
GPIO pin mapping
PA1 ETH_REF_CLK
PA2 ETH_MDIO
PA7 ETH_CRS_DV
PB13 ETH_TXD1
PC1 ETH_MDC n/a
PC4 ETH_RXD0
PC5 ETH_RXD1
PG11 ETH_TX_EN
PG13 ETH_TXD0
Enable
ICMP option
code
while (1)
{
/* USER CODE END WHILE */
MX_LWIP_Process();
/* USER CODE BEGIN 3 */
}
so i required UDP based example on STM32h743zi series.
if have you so please provide us
Reguard's
Hiren
2020-05-25 10:38 PM
Why you don't using RTOS? It much easyer to do with RTOS.
As I said above look after example which I linked, there complete lwip stack works. If one one CubeMX is broken then drop cube and use that example as starting point.
2020-05-25 11:53 PM
Also see https://community.st.com/s/question/0D50X0000C6eNNSSQ2/bug-fixes-stm32h7-ethernet. If you use the code there, please post there it's working for you or any questions.
2020-05-30 4:30 AM
> It much easyer to do with RTOS.
Oh, really? That's why ST's brainless code monkeys still haven't understood multi-threading since the year 2007, right? :) Actually, if one has a decent cooperative scheduler and software timers, then implementing lwIP for simple projects is easier without RTOS. But, if the project is complex or has real-time requirements, then it's "easier" to do it with RTOS.
2020-12-22 2:54 AM
Hi,
thanks for your comment,
can you please share your .ioc file (cube mx file )
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.