2019-01-02 3:46 AM
Hello and all good wishes for the new year!
While RM0433 has 4 bits reserved for FLASH_ACR_LATENCY, stm32h743xx.h only defined
#define FLASH_ACR_LATENCY_Msk (0x7U << FLASH_ACR_LATENCY_Pos)
What counts? Is bit3 in FLASH_ACR evaluated by the STM32H743 or not?
Solved! Go to Solution.
2021-10-21 6:06 AM
Hi @alister
You are right, I raised the request internally to align the github and the RM with the Cube firmware.
So, the defined of the FLASH_ACR LATENCY will be updated to 3 bits (instead of 4 bits).
Thanks for your contribution.
Imen
2019-01-02 5:08 AM
Will need to check my notes, but you should be able to do a write-readback check to see what gates were fabbed. I have parts that ran up to 533 MHz.
2019-01-03 6:37 AM
Hi @Uwe Bonnes ,
All the best for 2019 :smiling_face_with_smiling_eyes:
The header file is correct: The "FLASH_ACR -> LATENCY" bit-field is mapped on 3 bits.
-> The reference manual will be updated accordingly.
Many thanks for your continuous valuable feedback!
Khouloud.
2021-10-18 12:35 AM
RM0433 Rev 7 still says FLASH_ACR LATENCY is 4 bits and every version of stm32h743xx.h on github says FLASH_ACR_LATENCY_Msk 4 bits too.
@Khouloud GARSI or @Imen DAHMEN, could you confirm please?
2021-10-21 6:06 AM
Hi @alister
You are right, I raised the request internally to align the github and the RM with the Cube firmware.
So, the defined of the FLASH_ACR LATENCY will be updated to 3 bits (instead of 4 bits).
Thanks for your contribution.
Imen
2021-10-21 2:35 PM
Hi @Imen DAHMEN
I have a problem in production that may depend on this.
Is this the exact correction to the STM32H7 FLASH_ACR documentation please?
Bits 31:6 reserved
Bits 5:4 WRHIGHFREQ
Bit 3 reserved
Bits 2:0 LATENCY
Thanks
Alister
2021-10-22 3:17 AM
Hi @alister ,
In the "FLASH access control register (FLASH_ACR)" section, the table's Bit 3 should be marked as "reserved" + replace the description of this bit-field:
1111: 15 wait states used to read from non-volatile memory
by
0111: seven wait states used to read from non-volatile memory
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.