2018-07-11 2:56 AM
Hi,
I'm currently working on a project that needs to 'Read' a File in SDCARD.
My MCU is STM32H743XI, and the base for the project, I modified the FatFS uSD standalone application example in Cube FW for H7 V1.2.0, for STM32H743I-EVAL board.
I'm not using the Eval board for the project, so what I've done is; remove MFX I/O related codes from BSP sd.c driver file.
I've tested the project on my own board and it worked as expected when I use 2GB SD card, but it failed at f_open() when I use 4GB SD card.
So I searched this forum and found
https://community.st.com/0D50X00009Xkh8DSAR
, and modified SD_InitCard() function in stm32h7xx_hal_sd.c and inserted CMD1 code like below. The Bold line is changed.static uint32_t SD_InitCard(SD_HandleTypeDef *hsd)
{ HAL_SD_CardCSDTypedef CSD; uint32_t errorstate = HAL_SD_ERROR_NONE; uint16_t sd_rca = 1; /* Check the power State */ if(SDMMC_GetPowerState(hsd->Instance) == 0) { /* Power off */ return HAL_SD_ERROR_REQUEST_NOT_APPLICABLE; } if(hsd->SdCard.CardType != CARD_SECURED) {/* Send CMD2 ALL_SEND_CID */
errorstate = SDMMC_CmdSendCID(hsd->Instance); if(errorstate != HAL_SD_ERROR_NONE) { return errorstate; } /* Get Card identification number data */ hsd->CID[0] = SDMMC_GetResponse(hsd->Instance, SDMMC_RESP1); hsd->CID[1] = SDMMC_GetResponse(hsd->Instance, SDMMC_RESP2); hsd->CID[2] = SDMMC_GetResponse(hsd->Instance, SDMMC_RESP3); hsd->CID[3] = SDMMC_GetResponse(hsd->Instance, SDMMC_RESP4); }if(hsd->SdCard.CardType != CARD_SECURED)
{ /* Send CMD3 SET_REL_ADDR with argument 0 */ /* SD Card publishes its RCA. */ errorstate = SDMMC_CmdSetRelAdd(hsd->Instance, &sd_rca); if(errorstate != HAL_SD_ERROR_NONE) { return errorstate; } } if(hsd->SdCard.CardType != CARD_SECURED) { /* Get the SD card RCA */ hsd->SdCard.RelCardAdd = sd_rca; /* Send CMD9 SEND_CSD with argument as card's RCA */ errorstate = SDMMC_CmdSendCSD(hsd->Instance, (uint32_t)(hsd->SdCard.RelCardAdd << 16U)); if(errorstate != HAL_SD_ERROR_NONE) { return errorstate; } else { /* Get Card Specific Data */ hsd->CSD[0U] = SDMMC_GetResponse(hsd->Instance, SDMMC_RESP1); hsd->CSD[1U] = SDMMC_GetResponse(hsd->Instance, SDMMC_RESP2); hsd->CSD[2U] = SDMMC_GetResponse(hsd->Instance, SDMMC_RESP3); hsd->CSD[3U] = SDMMC_GetResponse(hsd->Instance, SDMMC_RESP4); } } /* Get the Card Class */ hsd->SdCard.Class = (SDMMC_GetResponse(hsd->Instance, SDMMC_RESP2) >> 20); /* Get CSD parameters */ HAL_SD_GetCardCSD(hsd, &CSD);/* Select the Card */
errorstate = SDMMC_CmdSelDesel(hsd->Instance, (uint32_t)(((uint32_t)hsd->SdCard.RelCardAdd) << 16)); if(errorstate != HAL_SD_ERROR_NONE) { return errorstate; } //20180710 SDMMC_CmdOpCondition(hsd->Instance, 0x40000000);//0xC0100000);//0x40000000);//0x00000000);//0x40000000);
/* All cards are initialized */
return HAL_SD_ERROR_NONE;}Here's My Questions:
1. After I changed the code, 4GB SD Card works, but total file-read speed has been significantly slowed down.
(It took 70 'seconds' after the debugging, before the modification it took 1 second when I used 2GB SD card.) Can you tell me why?
2. As you can see, I've tested with variety of arguments for CMD1. I know the [30:29] have to be [1:0], but it seems it doesn't matter. I've tried 0, 0xFFFFFFFF, but 4GB SD card still works.I don't understand why.
3. My Previous board used STM32F743NI MCU and I used SDCARD before, and didn't have any trouble with capacity of SD Card I was using. I assumed SD card initialization is not properly working now, but can't see any critical differences between H7 and F7 HAL Library. What should I do to regain the f_read speed using H7 library?
Thank you in advance.
#fatfs #sd-card #stm32h72018-07-11 8:53 AM
I really can't root-cause your specific issue, as it would involve a lot of my time. I have SD/MMC and eMMC working on the platform. The ST code may well have issues currently with low capacity SD or early V2/SDHC cards.
When porting from the EVAL board make sure to consider the bus transceiver and additional pins that uses, and the USE_SD_TRANSCEIVER define.
2018-07-11 9:21 PM
Hi, Thank you for your reply.
Is USE_SD_TRANSCEIVER define related with H/W spec? I don't use 1.8V but didn't change USE_SD_TRANSCEIVER define, which was set to 1U.
2018-07-11 9:44 PM
The USE_SD_TRANSCEIVER set to 1 implies the hardware is there. If you have done your own board and it is not there set it to 0.
2018-07-11 9:59 PM
Turns out USE_SD_TRANSCEIVER was defined at 2 different spot in the project. I only changed 1 of them, so I set both to 0 and project works without CMD1 code.
Thank you all.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.