2023-11-07 11:01 PM
Hi,
I'm working on enabling ETH on STM32H563. I tried to create a FW to do basic ping/ICMP in order to test the interface along with the PHY/switch chip. I found whenever I start the DMA by calling HAL_ETH_Transmit, it always returns HAL_ERROR due to timeout. I checked the status register, ETH_DMADSR and found TPS0 is set to 0x6, which indicates descriptor is not available or buffer underrun. I checked the descriptor and buffer with GDB and found nothing suspicious. Is there anything I should check?
Thank you.
Solved! Go to Solution.
2023-11-23 7:08 AM
Hello @minchingho_span and welcome to the community :),
The issue is currently under investigation .
Internal ticket number: 166429 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-23 7:08 AM
Hello @minchingho_span and welcome to the community :),
The issue is currently under investigation .
Internal ticket number: 166429 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-26 6:42 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.