2018-09-21 10:16 AM
Hi,
The current repository STM32Cube_FW_F7_V1.12.0 has for the full demo version the version 1.0.0 (STM32769I-EVAL_DEMO_V1.0.0_FULL.hex) . This version of the demo seems to have some problems. A new board has now the version 1.2.0. Where can I find this hex file?
thanks
2018-09-24 2:31 AM
Hello @Edgar ,
What are the encountered problems with this version of demo STM32769I-EVAL_DEMO_V1.0.0_FULL.hex ?
May be you should follow the readme file which noted for STM32769I-EVAL_DEMO_V1.0.0_FULL.hex binary, it is recommended to use an USB Key containing only set of media files available under "Utilities/Media" folder.
Kind Regards,
Imen
2018-09-24 5:25 AM
>>What are the encountered problems with this version of demo STM32769I-EVAL_DEMO_V1.0.0_FULL.hex ?
the original question seems to suggest that the version printed on the screen doesn't reflect the version that was on the board when it was delivered. ie code in .HEX reports 1.0.0 and respondent originally saw 1.2.0 and wants *that* hex file.
One can use the ST-LINK Utilities to download .BIN and .HEX files from a board.
2018-09-24 5:34 AM
00004E60 : 53 70 65 65 64 00 00 00 - 46 69 72 6D 2E 56 65 72 Speed...Firm.Ver
00004E70 : 00 00 00 00 20 53 54 4D - 33 32 37 36 39 49 2D 00 .... STM32769I-.
00004E80 : 20 20 20 20 45 56 41 4C - 20 20 20 00 20 53 54 4D EVAL . STM
00004E90 : 33 32 46 37 00 00 00 00 - 20 32 30 30 4D 48 7A 00 32F7.... 200MHz.
00004EA0 : 56 31 2E 30 2E 30 00 00 - 43 6F 70 79 72 69 67 68 V1.0.0..Copyrigh
00004EB0 : 74 20 28 63 29 20 53 54 - 4D 69 63 72 6F 65 6C 65 t (c) STMicroele
00004EC0 : 63 74 72 6F 6E 69 63 73 - 20 32 30 31 36 00 00 00 ctronics 2016...
2018-09-27 3:03 PM
000B66A0 : 43 50 55 20 53 70 65 65 - 64 00 00 00 46 69 72 6D CPU Speed...Firm
000B66B0 : 2E 56 65 72 00 00 00 00 - 20 53 54 4D 33 32 37 36 .Ver.... STM3276
000B66C0 : 39 49 2D 00 20 20 20 20 - 45 56 41 4C 20 20 20 00 9I-. EVAL .
000B66D0 : 20 53 54 4D 33 32 46 37 - 00 00 00 00 20 32 30 30 STM32F7.... 200
000B66E0 : 4D 48 7A 00 56 31 2E 32 - 2E 30 00 00 43 6F 70 79 MHz.V1.2.0..Copy
000B66F0 : 72 69 67 68 74 20 28 63 - 29 20 53 54 4D 69 63 72 right (c) STMicr
000B6700 : 6F 65 6C 65 63 74 72 6F - 6E 69 63 73 20 32 30 31 oelectronics 201
https://drive.google.com/open?id=1d3suP4Eb4Kr-EHDDIIfSjD4kleRhcktI
2018-10-25 8:51 AM
Hi Clive,
thanks for your answer. I realized now the files too.
On which way can I read and save the firmware from the STM32F769i-EVAL?
I have two new boards and these have the new firmware 1.2.0 too.
I tried with the st-link utility. But I can read only the 0x800000 flash addresses. Is it possible with the ST-LINK utility to read the 0x900000000 range. Can I do that with the command line options?
2018-10-25 9:08 AM
You'd have to check-box the External Loader via that menu selection. Then it will support the external NOR, etc. I did download a copy, but don't recall it having much useful content.
I've used the STM32 Cube Programmer app to download and save to a file through it's command line, as the GUI app doesn't appear to support saving to a file. I think I can save a log. I'm honestly confused who designed the user interface for this application.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.