2014-06-16 4:41 AM
Hello,
I downloaded ''STM32F4x7_ETH_LwIP_V1.1.0'' package and I want to make ''httpserver_socket'' example working with no success.I am getting hardfault ISR !I want to ask if there is somebody who succeeded to make it running.Thanks in advance for help.PS: my hardware is working fine since one of the standalone examples is working fine.Cheers #ethernet-freertos
2014-06-16 5:08 AM
So look at your unspecified compiler/tool-chain, and examine the instructions that are actually faulting?
2014-12-06 5:32 AM
Dear ST supporter,
Could you please confirm at least that there is an issue with STM32F4x7_ETH_LwIP_V1.1.0\Project\FreeRTOS\httpserver_socket example. I am getting hardfault? My hardware/jumpers are ok (I have tested standalone example and it is ok).Is there a new version of the package. I am using V1.1.0 31-July-2013?Thanks,2014-12-06 6:05 AM
Dear ST supporter,
It is worth to mention that I am using IAR EWARM V7.Waiting for your confirmation...Cheers,2014-12-06 3:15 PM
In anticipation of no other responses..
Might I suggest you learn how to implement and use a Hard Fault Handler.2014-12-09 1:37 AM
Dear Clive1,
I know how to do this task if there is no RTOS but with RTOS is more complicated.That's why I would prefer to have confirmation from ST other than debugging freeRTOS.Do you have the same ?2014-12-09 3:15 AM
Hello,
The application \STM32F4x7_ETH_LwIP_V1.1.0\Project\FreeRTOS\httpserver_socket was tested with the environment below (extract from the package release notes).
Now to be able to support you could you provide more details about your set-up:
Could you also describe better the issue you are facing, at which step the hard fault is generated? If you test another FreeRTOS based application, it will fail as well?
Development Toolchains and Compilers
IAR Embedded Workbench for ARM (EWARM) toolchain V6.50 + ST-Link
RealView Microcontroller Development Kit (MDK-ARM) toolchain V4.60 + ULINK
Raisonance IDE RIDE7 (RIDE) toolchain (RIDE7 IDE:7.40, RKitARM for RIDE7:1.48) + Rlink Pro
Atollic TrueSTUDIO toolchain V4.0.0 + ST-LINK
TASKING VX-toolset for ARM Cortex-M V4.4r1 + ST-LINK
Supported Devices and EVAL boards
STM32F407xx/STM32F417xx devices and STM324xG-EVAL board
STM32F427xx/STM32F437xx devices and STM324x7I-EVAL board
regards,
Jasmin.
2014-12-11 5:31 AM
Hello Jasmin,
Here my answers:Now to be able to support you could you provide more details about your set-up:o STM32F4 device and its revision => Device ID:0x413, Device flash Size : 512KBytes, Device family, STM32F40xx/F41xxo EVAL board and its version: => STM3240G-EVALo EWARM version => IAR EWARM 6.70Could you also describe better the issue you are facing, at which step the hard fault is generated? ==> Call stack gives: PendSV => vTaskSwitchContext => HardfaultIf you test another FreeRTOS based application, it will fail as well?==> All freeRTOS applications fail2014-12-17 6:02 AM
Hi Jasmin,
Any update about the subject ?Can I consider this silence as a confirmation for the problem with the application?2014-12-17 6:50 AM
Can I consider this silence as a confirmation for the problem with the application?
Consider it's just very low priority. If you need it fixed you'll probably need to do it yourself. Are you a student or a developer?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.