2020-08-06 6:56 PM
2020-08-07 12:09 AM
Hi Victor,
What should that make sense for?
LD5/LD6 can only be influenced indirectly by the STM32F429, indicating VBUS and overcurrent at the OTG port.
Best regards
/Peter
2020-08-07 2:17 AM
Hi Peter,
For other purposes not using VBUS and OTG.
---Victor
2020-08-07 2:21 AM
Oh, we cannot use the VBUS that is output of STMPS2141STR.
But the /Fault is open drain though.
2020-08-07 2:56 AM
Well, you could expand the BSP yourself, if you really want to drive LD6. But you have to keep in mind that it is being driven with some kind of wired-or with the STMPS2141, so the status of LD6 depends on OTG_FS_OC and the /FAULT signal from the STMPS2141.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.