2020-08-12 12:58 PM - last edited on 2025-09-18 4:01 AM by Andrew Neil
bootloader update the application saved on the USB memory stick attached to on STM32F429 Discovery board when reset occurs, it detects if USB flash memory pen is attached, if attached read and copy application file (hexfile) from usb and update
If reset happens or the board is powered up -> boot loader checks if usb flash memory is attached to the usb port , -> if attached-> check if there is firmware stored in the usb flash memory pen ->is so copy and update the application from usb stick-> then jump to the application which has been updated from the flash memory -> end.
Thanks I really appreciate of you can help me with this thanks.
Solved! Go to Solution.
2020-08-12 1:02 PM
What's the question?
STM32Cube_FW_F4_V1.25.0\Projects\STM32F429I-Discovery\Applications\USB_Host\FWupgrade_Standalone
2020-08-12 1:02 PM
What's the question?
STM32Cube_FW_F4_V1.25.0\Projects\STM32F429I-Discovery\Applications\USB_Host\FWupgrade_Standalone
2020-08-12 2:15 PM
Hi Clive ,
I think you have answered my question , so the code you pointed dose exactly what I need ? if so I will be speechless and will have to create a new word Thanking you ! ...
2020-08-12 2:18 PM
I think this uses .BIN files, but could be adapted to handle .HEX or .DFU files.
2020-08-12 2:22 PM
I can handle this , it was just the code and the mechanism I needed to have ... appreciate your help , Thanks you very very very much! really
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.