2022-01-26 4:19 AM
I am using an stm32f401rc microcontroller, peripheral USB mass storage host is not detected, I am generating code as per the USB MSC HOST labs document.
MX_USB_HOST_Process();
switch(Appli_state)
{
case APPLICATION_IDLE:
break;
case APPLICATION_START:
HAL_UART_Transmit(&huart6,"APPLICATION_START\r\n",strlen("APPLICATION_START\r\n"),1000);
if(f_mount(&myUsbFatFS, (TCHAR const*)USBHPath, 0) == FR_OK)
HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_SET);
break;
case APPLICATION_READY:
HAL_UART_Transmit(&huart6,"APPLICATION_READY\r\n",strlen("APPLICATION_READY\r\n"),1000);
if(HAL_GPIO_ReadPin(BUTTON_GPIO_Port, BUTTON_Pin) == GPIO_PIN_SET)
if(UsbTest_Write())
HAL_GPIO_WritePin(LED4_GPIO_Port, LED4_Pin, GPIO_PIN_SET);
else
HAL_GPIO_WritePin(LED3_GPIO_Port, LED3_Pin, GPIO_PIN_SET);
HAL_Delay(1000);
break;
case APPLICATION_DISCONNECT:
HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_RESET);
break;
}
the application starts but the application-ready message have not occurred.
Regards,
naren
2022-01-26 7:14 AM
Hello @Nredd.1 ,
Try to increase heap and stack sizes in the CubeMx setting.
Maybe you should check the pins configuration, check if D+/D- are not swapped !
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen
2022-01-27 3:51 AM
Thanks,
It is working with external CLK settings,
the USB hid device's barcode scanner is working fine, but some hid devices is not working(keyboard and mouse)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.