2015-07-11 9:00 AM
Good evening at all.
I'm trying to port the CustomHID_Standalone example from STM324xG_EVAL example application in latest HAL driver to the STM32F4-Discovery board. I successfully get no errors in compiling the firmware (adapted to use stm32f4_discovery.c) and other files relative to the specific board and it is recognized from windows, but not ENUMERATED.Anyone had success in this task?However, anyone as a correctly ported example from STM324xG_EVAL to STM32F4-DISCOVERY to share? It could be a nice starting point for my project.Thank you all in advance. #stm32f4-disco #hal #usb #hid2015-07-11 12:50 PM
Make sure the HSE_VALUE and PLL settings reflect that the DISCO board has an 8 MHz source, vs the 25 MHz of the EVAL
2015-07-12 3:18 AM
This was exactly the problem. Thank you very much clive1!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.