2017-03-10 6:39 AM
Hello ;
I tried to read the reference manual but still not clear ;
is it possible to use USB FS ( GPIOA ) and USB_ hs ( FS mode) ( GPIOB) at same time in host mode ?
in our applicstion we need two host USB to communicate with 2 USB flash ( FATFS)
Thank you
Regards
#usb-stm32f4-stm32f72017-03-10 9:43 PM
Hi,
I have no actual experience in coding USB,so I cant answer exact questions about it,
but I believe that you need to run a single USB Host 'supporting all classes' connected to a USB HUB.
then you can have 2/3/4 USB Flash Drives and or a mouse or printer if you want to.
2017-06-16 3:01 AM
Hi
ASSAAD.ASSAAD
,Indeed. You may use the two USB peripherals on GPIOA and GPIOB simultaneously.
Khouloud.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.