2017-10-09 3:18 PM
Hi,
I've a question regarding the HAL UART Environment. I could observe that the Interrupt are raised sometimes 2x although I'm sending only one Byte for the STM32 where I'm reading each single byte.
At which conditions can this happen?
#cube-hal #stm32 #uart-it2017-10-09 5:32 PM
Perhaps you can illustrate with some code and diagrams?
Does this occur on a continuous basis, or just when you first initialize the USART?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.