2015-02-27 7:31 AM
Has any body rebuilt the STM32F107 LwIP TCP/IP demo (STSW-STM32026) in latest IAR EWARM toolchain ? The demo provided by ST still uses IAR 5.42 ( old one). This creates errors when I try to rebuild with IAR 6.30. Any suggestions ?
#ethernet #stm32f1072015-02-27 8:04 AM
Any suggestions ?
Read what the error messages tell you, and address/fix those issues? Start with the first ones and move forward incrementally. Start with the obvious project related issues like defines and include paths.2015-02-27 10:24 AM
Hi Clive1, thanks for your quick reply & interest. Let us talk about errors I get !
Earlier I noticed that it concerned with only core_cm3.h file so I replaced it with new one . Then if I rebuild the same I get following errors - Error[Pe065]: expected a '';'' C:\ST projects\stsw-stm32026-TCPIP\STM32F107_ETH_LwIP_V1.0.0\Libraries\CMSIS\Core\CM3\core_cm3.h 896 The code is - /** \brief Set Priority Grouping This function sets the priority grouping field using the required unlock sequence. The parameter PriorityGroup is assigned to the field SCB->AIRCR [10:8] PRIGROUP field. Only values from 0..7 are used. In case of a conflict between priority grouping and available priority bits (__NVIC_PRIO_BITS) the smallest possible priority group is set. \param [in] PriorityGroup Priority grouping field */ static __INLINE (cursor is here
)void NVIC_SetPriorityGrouping(uint32_t PriorityGroup) { uint32_t reg_value; uint32_t PriorityGroupTmp = (PriorityGroup & (uint32_t)0x07); /* only values 0..7 are used */ reg_value = SCB->AIRCR; /* read old register configuration */ reg_value &= ~(SCB_AIRCR_VECTKEY_Msk | SCB_AIRCR_PRIGROUP_Msk); /* clear bits to change */ reg_value = (reg_value | ((uint32_t)0x5FA << SCB_AIRCR_VECTKEY_Pos) | (PriorityGroupTmp << 8)); /* Insert write key and priorty group */ SCB->AIRCR = reg_value; } As this is core CMSIS file, I do not think there is an error ! What is your opinion ? Well, I also appeal to ST people to change the demo files so that it can be rebuilt without any errors with latest & not so latest version of IAR. ( the demos are of 2009 !) Thanks.2015-02-27 11:58 AM
Well, I also appeal to ST people to change the demo files so that it can be rebuilt without any errors with latest & not so latest version of IAR. ( the demos are of 2009 !)
Isn't this really IAR's problem, they after all released an IDE incapable of compiling projects from an earlier version? Do they offer a migration guide? Or support? A compatibility check box? I'd look at how the __INLINE macro is defined.
2015-02-28 12:27 AM
__INLINE define in file core_cm3.h
........
#elif defined ( __ICCARM__ )
#define __ASM __asm /*!< asm keyword for IAR Compiler */
#define __INLINE inline /*!< inline keyword for IAR Compiler. Only available in High optimization mode! */
#define __STATIC_INLINE static inline
......
I added the macro __INLINE to my project function and it works without compiler errors with IAR EWARM 7
Check the compiler options settings dialogWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.