2018-06-05 12:20 AM
Hello everyone,
I am having a little issue with my STM32F103RBT6 code. I am trying to make the Receive CAN IT work.
The problem I am facing is that it is working for a small amount of time and then just stops (either it's because of the overflow I don't know how to deal with or because the IT just won't retrigger).
My code is looking like this :
in main :
int flag2 = 0;
while (1)
{if(!flag2) // RECEIVE
{
HAL_CAN_Receive_IT(&hcan, CAN_FIFO0);
flag2 = 1;
}
for(cpt_for = 0; cpt_for<CAN_nb_trames_Rx_cc ; cpt_for++) // Receive test { // This is for me to see if the received messages are what I was expecting TxMessage.DLC = CAN_Tab_RxMessages[cpt_for].DLC; TxMessage.Data[0] = CAN_Tab_RxMessages[cpt_for].Data[0]; TxMessage.Data[1] = CAN_Tab_RxMessages[cpt_for].Data[1]; TxMessage.Data[2] = CAN_Tab_RxMessages[cpt_for].Data[2]; TxMessage.Data[3] = CAN_Tab_RxMessages[cpt_for].Data[3]; TxMessage.Data[4] = CAN_Tab_RxMessages[cpt_for].Data[4]; TxMessage.Data[5] = CAN_Tab_RxMessages[cpt_for].Data[5]; TxMessage.Data[6] = CAN_Tab_RxMessages[cpt_for].Data[6]; TxMessage.Data[7] = CAN_Tab_RxMessages[cpt_for].Data[7]; TxMessage.ExtId = CAN_Tab_RxMessages[cpt_for].ExtId; TxMessage.IDE = CAN_Tab_RxMessages[cpt_for].IDE; TxMessage.RTR = CAN_Tab_RxMessages[cpt_for].RTR; TxMessage.StdId = CAN_Tab_RxMessages[cpt_for].StdId; hcan.pTxMsg = &TxMessage; HAL_CAN_Transmit(&hcan, 100); }
}
void HAL_CAN_RxCpltCallback(CAN_HandleTypeDef *hcan)
{
CAN_Tab_RxMessages[hcan->pRxMsg->FMI]=*(hcan->pRxMsg); flag2 = 0;}
When I compile and implement it, it works perfectly when I try to receive just one CAN frame. But if I try to receive 2 at the same time it will stop. By reducing the speed of the frames I try to receive (should be 1 every 10ms but I tried 1 every 1 second), it works. However, if I send these 2 frames (that I am supposed to receive) at the same time, my �C won't receive them anymore, and if I dive into the registers, I can see that the Receive interrupt is not active anymore (hence it is not in interrupt mode). In the end, when I tried to receive two frames that were coming at a higher speed (1 every 10 ms), the issue I was facing was that the overflow bit was set in the CAN register and I don't really know how to deal witht this issue either.
If you have any idea on how I can fix it !
In advance thanks !
PS : On a side note, I am also looking for a board with a STM32F4 on it (I'm interested in its 2 CAN) where the 2 CAN inputs/outputs are available (for example in the discovery board, one is connected to the USB, which doesn't suit me). So if anyone knows a board that could fit my needs !
#hal_can_receive_it #stm32f103-interrupt2018-06-05 5:21 AM
So, by trying different things in order to make my code work, I changed my RxCallback function to :
void HAL_CAN_RxCpltCallback(CAN_HandleTypeDef *hcan)
{
CAN_Tab_RxMessages[hcan->pRxMsg->FMI]=*(hcan->pRxMsg);
__HAL_CAN_ENABLE_IT (hcan, CAN_IT_FMP0);}and using :
__HAL_CAN_ENABLE_IT (&hcan, CAN_IT_FMP0);
just before my while(1). And now it seems to be working !
However, I am still interested in your feedback on this method, is it right ? Do you think there is a more proper way to do it ? Was my code supposed to work in the first place ?
In advance, thank you !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.