2015-08-28 2:06 AM
Hi. I am using STM32F070CB with libraries STM32F10x_L1xx_F3xx_USBL(v4.0.0) and STM32F0xxSPL(v1.1.0) to implement custom HID to implement simple hello world(PC sends 64 bytes and MCU sends back the same 64 bytes)
The example code worked perfectly for STM32F103CB. I ported the same project for STM32F070CB with changing parts only related to IO configuration(set to AF), clock configuration(system, peripheral, and USB), and interrupts. When I connect the programmed board to PC, it is recognized as Unknown device. Am i supposed to use different library or I need to change something else?Thank you #usb #adc #noise #stm32f070We’re moving the ST Community to a new platform to give you a better and more reliable community experience.