2015-07-13 9:16 PM
When creating USB CDC code for devices with a USB FS port, 448 bytes are wasted. The USBD_CDC_HandleTypeDef structure in usbd_cdc.h uses CDC_DATA_HS_MAX_PACKET_SIZE to create data buffer. This is defined as 512 bytes(message size for USB HS). But, the CDC_DATA_FS_MAX_PACKET_SIZE define can be used for USB FS devices, which only requires 64 bytes.
ST should modify code to check if USB is FS or HS. #stm32cube #usb #cdc #com-portWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.