cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMonitor-UCPD does not recognize ON-FUSB3-STM32. VCP does not appear when I plug Micro USB to ON-FUSB3-STM32.

TKwon.2
Associate

When I try to using STM32CubeMonitor-UCPD software with X-CUBE-USB-PD and ON-FUSB3-STM32, VCP does not appear on the laptop. I cannot see any connected board on the software.

I already installed STM32CubeMonitor-UCPD and USB driver for ST-LINK.

And, downloaded X-CUBE-USB-PD project on ON-FUSB3-STM32.

Is there any required modification on X-CUBE-USB-PD project? for using STM32CubeMonitor-UCPD with ON-FUSB3-STM32.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Yohann M.
ST Employee

Dear @TKwon.2​

X-CUBE-USBPD V3.1.0 contains an application using STM32CubeMonitor-UCPD.

You should take as reference the following application (Link on github) done on ON-FUSB3-STM32.

Idea is to connect PA0 and PA1 from EVAL board to your VCP pins available on your ST link.

Configuration is defined in 'tracer_emb_conf.h':

#define TRACER_EMB_USART_INSTANCE                    USART4
 
#define TRACER_EMB_TX_GPIO                           GPIOA
#define TRACER_EMB_TX_PIN                            LL_GPIO_PIN_0
#define TRACER_EMB_RX_GPIO                           GPIOA
#define TRACER_EMB_RX_PIN                            LL_GPIO_PIN_1

Regards,

Yohann

View solution in original post

2 REPLIES 2
Yohann M.
ST Employee

Dear @TKwon.2​

X-CUBE-USBPD V3.1.0 contains an application using STM32CubeMonitor-UCPD.

You should take as reference the following application (Link on github) done on ON-FUSB3-STM32.

Idea is to connect PA0 and PA1 from EVAL board to your VCP pins available on your ST link.

Configuration is defined in 'tracer_emb_conf.h':

#define TRACER_EMB_USART_INSTANCE                    USART4
 
#define TRACER_EMB_TX_GPIO                           GPIOA
#define TRACER_EMB_TX_PIN                            LL_GPIO_PIN_0
#define TRACER_EMB_RX_GPIO                           GPIOA
#define TRACER_EMB_RX_PIN                            LL_GPIO_PIN_1

Regards,

Yohann

Thank you for your reply. Now, it works.

Based on your reply, I realized VPC is the function of ST link​.

I thought VCP is the function of MCU Which connect to the laptop directly without RS-232 Transceiver IC.

At first, I have some difficulties because I used ST link V2 which does not support VCP.

I changed to ST link V3, now it works.

Anyway, thanks again.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.