2020-03-19 5:13 PM
Hi,
I am trying to use the latest CubeIDE V1.3 with cubeMX v5.6 with FatFS R0.12c and with FreeRTOS cmsis_osv2 (tried it with cmsis_osv1 too but to same). I am using FreeRTOS in my project. The SD card is connected using SDIO 1-bits (SD 1 bit because MMC 1 bit doesnt work with fatfs) wide bus. The MCU is STM32L151RDT6. HAL driver is V1.9.
The problem is that f_mount function is never working.
I tried without Freertos, it is work fine but FREERTOS+SDIO+FATFS f_mount doesnt work.
If I using cmsis_v2 I have compiling error after generating code from MX.
undefined reference to `osSemaphoreCreate' syscall.c Middlewares/Third_Party/FatFs/src/option line 45 C/C++ Problem
undefined reference to `osSemaphoreWait' syscall.c Middlewares/Third_Party/FatFs/src/option line 84
because in cmsis_osv2 osSemaphoreCreate is renamed to osSemaphoreNew and osSemaphoreWait to osSemaphoreAcquire.
I fixed it with :
osSemaphoreId_t SEM;
....
SEM = osSemaphoreNew(1,0, &SEM_attributes);
...
if(osSemaphoreAcquire(SEM,_FS_TIMEOUT) == osOK)please help.
Thank you
2020-04-30 10:07 PM
I have exactly the same problem. Is anyway I can walk-around?
Thanks.
2020-10-05 6:41 PM
Hi,
I've got the same problem. Was anyone able to fix it?
Thanks!
2020-10-05 9:31 PM
Got around this issue by choosing the freertos interface CMSIS v1 instead of CMSIS V2
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.