2017-04-19 10:40 AM
I'm testing STM32F746GZ for our new project now. I use STM32CubeMx V4.20.0 with FW_F7 V1.6.1 generated a empty project for Nucleo- F746ZG board as MDK-ARM V5 project. There was no any problem if I use HSI as system clock PLL source(default).
However, after I enabled and switched system PLL clock source to HSE in byPASS mode(default 8MHz MCO on Nucleo-F746ZG), it stopped working inside 'SystemClock_Config()'.
My case is very easy to be duplicated if you have a Nucleo-F746ZG board.
I believe STM32Cube has a bug for running HSE on F7 processor. It would be very appreciated if any body over there can help fixing this issue.Thank you in advance.
Ian
#stm32f7 #stm32cube-bug #clock-configuration #hse-issue2017-04-19 4:19 PM
change RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI | RCC_OSCILLATORTYPE_HSE;
to
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
when using the external oscillator i choose 'crystal/ceramic resonator' rather than bypass. i think bypass is for when you're using something like an si5351a to generate clock signals. I am pretty new to all this so I could be wrong.
2017-04-20 1:07 AM
Hello
Jin.Ian
,Please switch to the new CubeMX version (4.1) where the regression bug faced with the version 4.0 is fixed.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-04-20 8:15 AM
The default HSE for
Nucleo-F746ZG board is the 8MHZ MCO from ST/LINK (U2), So have to config the RCC-HSE as BYPASS Clock Source.
There is no real crystal resonator assembled on that board.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.