2020-01-26 8:36 PM
STM32 lwip stack issue - frames/not received/processed - FBE error
FBE bit 12 -Fatal bus error. STM board used : STMh743
is there any timing problem or a configuration problem with the clock, bus speed or DMA?
2020-06-02 8:49 PM
Hi Anand,
Have you solve the problem? I encounter the same problem with you.
Best regards.
2020-06-02 11:26 PM
Oh, i solved the problem.
lwip mem_malloc zone should be in RAM3.
the macro LWIP_RAM_HEAP_POINTER should be defined with 0x30044000
and, MEM_LIBC_MALLOC should be zero
2020-06-04 5:41 AM
>the macro LWIP_RAM_HEAP_POINTER should be defined with 0x30044000
Instead, consider using the linker to place your variables at memory addresses. That's what the linker's for.
lwIP does this with LWIP_RAM_HEAP_POINTER:
ram = (u8_t *)LWIP_MEM_ALIGN(LWIP_RAM_HEAP_POINTER);No checks. The compiler can't know the linker hasn't placed something else there. You'd have to remember, and as your project grows and/or more developers join your team, that detail could be easily forgotten.
For example, take a look at my map file. If I'd defined that macro like that, my .EthDescriptorsBlock section would become corrupted.
.EthTxBlock 0x30040000 0x4e30
0x30040000 . = ALIGN (0x4)
0x30040000 __ETH_TX_START = .
*(.TxArraySection)
.TxArraySection
0x30040000 0x4e30 Common\Eth\LWIP\Target\ethernetif.o
0x30040000 lwip_custom_ram_heap
0x30044e30 __ETH_TX_END = .
.EthDescriptorsBlock
0x30044e30 0x5d0
0x30045000 . = ALIGN (0x400)
*fill* 0x30044e30 0x1d0
0x30045000 __ETH_DESCRIPTORS_START = .
*(.RxDecripSection)
.RxDecripSection
0x30045000 0x180 Common\Eth\LWIP\Target\ethernetif.o
0x30045000 DMARxDscrTab
*(.TxDecripSection)
.TxDecripSection
0x30045180 0x180 Common\Eth\LWIP\Target\ethernetif.o
0x30045180 DMATxDscrTab
0x30045400 . = ALIGN (0x400)
*fill* 0x30045300 0x100
0x30045400 __ETH_DESCRIPTORS_END = .If you're using GCC, take a look at my ethernetif.c and linker command file attached at https://community.st.com/s/question/0D50X0000C6eNNSSQ2/bug-fixes-stm32h7-ethernet for an example of how to use compiler attributes to get the linker to place the lwIP heap in RAM3.
2020-07-02 9:54 PM
not yet :( , we are in contact with stm colleagues to fix this.once i got the solution will inform you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.