cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 + EXPHY USB3300 + VBUS Sensing

KTarc
Associate II

Dear All.

Based on HAL library, I make small project where I have USB HS with external PHY (USB3300) and CDC class. Works well. What I need is to implement Vbus sensing. This can be done only via external phy, there are some flags in registers to enable it, but I don’t know how make it working. I got a few question:

1.      Can current HAL library enable vbus sensing in the USB3300 chip?

2.      Is it possible to have access to the ULPI communication to setup those registers and bit manually?

BR

KWT

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.