2024-11-08 3:34 PM - last edited on 2024-11-11 10:01 AM by Andrew Neil
I am trying to make a very simple SPI ISR to read the RXDR and store the value to a buffer. However, I cannot get the ISR to even trigger without using HAL_SPI_Receive_IT(). I do not want to use the callbacks or the default IRQ generated by cube. I currently just have the following in my ISR:
void spiISR(SPI_HandleTypeDef *hspi){
if (__HAL_SPI_GET_FLAG(&hspi1, SPI_FLAG_RXNE)) {
rxBuffer[rxIndex] = SPI1->RXDR;
// Increment index and wrap around if necessary
rxIndex = (rxIndex + 1) % RX_BUFFER_SIZE;
__HAL_SPI_CLEAR_OVRFLAG(&hspi1);
}
}
Since I don't want to use the generated IRQ I do this:
void SPI1_IRQHandler(void)
{
/* USER CODE BEGIN SPI1_IRQn 0 */
spiISR(&hspi1);
return;
/* USER CODE END SPI1_IRQn 0 */
HAL_SPI_IRQHandler(&hspi1);
/* USER CODE BEGIN SPI1_IRQn 1 */
/* USER CODE END SPI1_IRQn 1 */
}
I have turned on the following:
MX_SPI1_Init();
/* USER CODE BEGIN 2 */
HAL_NVIC_EnableIRQ(SPI1_IRQn);
__HAL_SPI_ENABLE_IT(&hspi1, SPI_IT_RXNE);
This would leave me to believe that the ISR should trigger when the fifo is not empty; however that is not the case.
I have ensured data is being transferred to the board on an oscilloscope, but the board shows no indication of receiving data
Solved! Go to Solution.
2024-11-11 12:33 PM
Thank you for the responses @PGump.1 and @gbm,
I have found that I needed to call __HAL_SPI_ENABLE(&hspi1); to get the interrupt to trigger however the data coming in seems random. I try sending 1-8 to this slave, and the data shows correctly on oscilloscope; however, I just get repeating sequences of:
64 192 224 1 1 1 129 1
20 12 14 8 16 16 24 16
Sometimes other randoms sequences appear too, I'm not seeing any correlation between these numbers. However, I will likely create a new post since this no longer pertains to the ISR not triggering.
2024-11-09 10:44 AM
Have you configured the SPI? Show the code.
2024-11-10 4:47 PM - edited 2024-11-10 5:13 PM
Hi,
Part of the problem is - you are not clearing the IRQ in your handler.
Oops - cancel the above - I was thinking of another brand device (not ST)...
Kind regards
Pedro
2024-11-11 9:31 AM
Hi @gbm ,
Here is my Initialization for the spi slave
static void MX_SPI1_Init(void)
{
/* USER CODE BEGIN SPI1_Init 0 */
/* USER CODE END SPI1_Init 0 */
/* USER CODE BEGIN SPI1_Init 1 */
/* USER CODE END SPI1_Init 1 */
/* SPI1 parameter configuration*/
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_SLAVE;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_2EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 0x0;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
hspi1.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
hspi1.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
hspi1.Init.TxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
hspi1.Init.RxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
hspi1.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
hspi1.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
hspi1.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
hspi1.Init.IOSwap = SPI_IO_SWAP_DISABLE;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SPI1_Init 2 */
/* USER CODE END SPI1_Init 2 */
}
2024-11-11 12:33 PM
Thank you for the responses @PGump.1 and @gbm,
I have found that I needed to call __HAL_SPI_ENABLE(&hspi1); to get the interrupt to trigger however the data coming in seems random. I try sending 1-8 to this slave, and the data shows correctly on oscilloscope; however, I just get repeating sequences of:
64 192 224 1 1 1 129 1
20 12 14 8 16 16 24 16
Sometimes other randoms sequences appear too, I'm not seeing any correlation between these numbers. However, I will likely create a new post since this no longer pertains to the ISR not triggering.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.