2021-03-09 3:35 AM
I have a problem with operating the traffic light from the class method - every time the program crashes at that point.
Here is a simplified example for understanding what I'm writing about:
Class:
class IO_control
{
int num;
public:
osSemaphoreId semaphoreHandle;
int *outputs;
IO_control(int num,int outputs,osSemaphoreId semaphoreHandle);
virtual ~IO_control();
void SetOutputs();
void UnsetOutputs();
};
/***********************************************/
IO_control::IO_control(int num, int *outputs,osSemaphoreId semaphoreHandle)
{
this->num = num;
this->outputs = outputs;
this->semaphoreHandle = semaphoreHandle;
}
IO_control::~IO_control(){}
void IO_control::SetOutputs()
{
osSemaphoreWait(semaphoreHandle, osWaitForever);
*outputs |= num;
osSemaphoreRelease(semaphoreHandle);
}
void IO_control::UnsetOutputs()
{
osSemaphoreWait(semaphoreHandle, osWaitForever);
*outputs &= ~(num);
osSemaphoreRelease(semaphoreHandle);
}I have three tasks that fight over one variable i_o_CAN.data_out, specifically four instances of the class + sending a message
two set it - the third copies it to the CAN message
typedef struct can_I_O_struct
{
union
{
int data_out;
uint8_t out_arr[4];
};
union
{
int data_in;
uint8_t in_arr[4];
};
} I_O_struct_can;
I_O_struct_can i_o_CAN;
osSemaphoreId CAN_IO_semaphoreHandle;
IO_control out1(1,&i_o_CAN.data_out,CAN_IO_semaphoreHandle);
IO_control out2(2,&i_o_CAN.data_out,CAN_IO_semaphoreHandle);
IO_control out3(3,&i_o_CAN.data_out,CAN_IO_semaphoreHandle);
IO_control out4(4,&i_o_CAN.data_out,CAN_IO_semaphoreHandle);
void Task01(void const * argument)
{
for(;;)
{
out1.SetOutputs();
osDelay(50);
out1.UnsetOutputs();
osDelay(1000);
out2.SetOutputs();
osDelay(50);
out2.UnsetOutputs();
osDelay(1000);
}
}
void Task02(void const * argument)
{
for(;;)
{
out3.SetOutputs();
osDelay(50);
out3.UnsetOutputs();
osDelay(2000);
out4.SetOutputs();
osDelay(50);
out4.UnsetOutputs();
osDelay(2000);
}
}
void TaskCAN_Tx(void const * argument)
{
int tmp = 0;
TxHeader2.StdId = 0x180;
TxHeader2.DLC = 4;
for(;;)
{
osSemaphoreWait(CAN_IO_semaphoreHandle, osWaitForever);
if (i_o_CAN.data_out != tmp)
{
tmp = i_o_regs_can.data_out;
TxData2[0] = i_o_CAN.out_arr[0];
TxData2[1] = i_o_CAN.out_arr[1];
TxData2[2] = i_o_CAN.out_arr[2];
TxData2[3] = i_o_CAN.out_arr[3];
if (HAL_CAN_AddTxMessage (&hcan2, &TxHeader2, TxData2, &TxMailbox2)!= HAL_OK)
{
Error_Handler ();
}
}
osSemaphoreRelease(CAN_IO_semaphoreHandle);
}
}when I adjust it so that I operate the traffic lights directly from the tasks, it works
void IO_control::SetOutputs()
{
*outputs |= num;
}
void IO_control::UnsetOutputs()
{
*outputs &= ~(num);
}
//////////////////////////////////////////////////////////////////////
void Task01(void const * argument)
{
for(;;)
{
osSemaphoreWait(CAN_IO_semaphoreHandle, osWaitForever);
out1.SetOutputs();
osSemaphoreRelease(CAN_IO_semaphoreHandle);
osDelay(50);
osSemaphoreWait(CAN_IO_semaphoreHandle, osWaitForever);
out1.UnsetOutputs();
osSemaphoreRelease(CAN_IO_semaphoreHandle);
osDelay(1000);
osSemaphoreWait(CAN_IO_semaphoreHandle, osWaitForever);
out2.SetOutputs();
osSemaphoreRelease(CAN_IO_semaphoreHandle);
osDelay(50);
osSemaphoreWait(CAN_IO_semaphoreHandle, osWaitForever);
out2.UnsetOutputs();
osSemaphoreRelease(CAN_IO_semaphoreHandle);
osDelay(1000);
}
}but in reality it's not that simple and I need to access the traffic light from insatnaci - in addition, it's a lot of useless code
Solved! Go to Solution.
2021-03-12 11:00 PM
STM32F205
but the problem is not related to hardware or freertos
I've found that it's a matter of C++ and bad passing of the reference to the class.
This is a functional solution:
class IO_control {
int num;
public:
osSemaphoreId & semaphoreHandle;
int * outputs;
IO_control (int num, int * outputs, osSemaphoreId & semaphoreHandle);
virtual ~IO_control();
void SetOutputs();
void UnsetOutputs();
};
/***********************************************/
IO_control::IO_control (int _num, int * _outputs, osSemaphoreId & _semaphoreHandle) :
num(_num), semaphoreHandle(_semaphoreHandle), outputs(_outputs) {
}
2021-03-12 3:16 AM
Hi @Luděk Urbani�? ,
Which product please?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-03-12 11:00 PM
STM32F205
but the problem is not related to hardware or freertos
I've found that it's a matter of C++ and bad passing of the reference to the class.
This is a functional solution:
class IO_control {
int num;
public:
osSemaphoreId & semaphoreHandle;
int * outputs;
IO_control (int num, int * outputs, osSemaphoreId & semaphoreHandle);
virtual ~IO_control();
void SetOutputs();
void UnsetOutputs();
};
/***********************************************/
IO_control::IO_control (int _num, int * _outputs, osSemaphoreId & _semaphoreHandle) :
num(_num), semaphoreHandle(_semaphoreHandle), outputs(_outputs) {
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.