2022-08-09 6:31 PM
In P687, right bottom part of Figure 248, it says "GRXFSIZ[31:16]", while P715 says that GRXFSIZ[31:16] is "Reserved, must be kept at reset value.".
Besides, also in Figure 248, it says "GNPTXFSIZ", but there is no such register in this Reference Manual.
I think "GRXFSIZ[31:16]" should be "GRXFSIZ[15:0]" and "GNPTXFSIZ" should be "HNPTXFSIZ/DIEPTXF0", which make sense in this context.
2022-08-10 4:24 AM
Hi @Rzh.1 and welcome to the Community :),
I confirm this issue:
Thank you for your contribution.
Internal ticket number: 132955 (This is an internal tracking number and is not accessible or usable by customers).
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.