2014-09-15 5:39 AM
USBD_CDC_TransmitPacket() function contains a bug:
it sets the 'transmission in progress' flag AFTER starting the actual transmission, so if the 'transmission done' interrupt happens too early, the flag will be set AFTER the interrupt and hence will never be cleared. To fix this, move ''hcdc->TxState = 1'' line before the call to USBD_LL_Transmit() :uint8_t USBD_CDC_TransmitPacket(USBD_HandleTypeDef *pdev)
{ USBD_CDC_HandleTypeDef *hcdc = pdev->pClassData; if(pdev->pClassData != NULL) { if(hcdc->TxState == 0) {/* Tx Transfer in progress */
hcdc->TxState = 1;
/* Transmit next packet */
USBD_LL_Transmit(pdev, CDC_IN_EP, hcdc->TxBuffer, hcdc->TxLength); return USBD_OK; } else { return USBD_BUSY; } } else { return USBD_FAIL; } }This bug
we found
in practice, and
it was described
#cdc #stm32 #usb #usb #usb #library #bug #cdc #stm32cube2014-09-16 7:27 AM
Hi kukhtin.sergey,
Thank you for bringing this issue to our attention. We'll pass it along to our development team. Keep an eye our for the next update!Regards.2014-12-24 3:32 AM
2015-10-05 4:55 AM
bug is still not fixed!
cost me half a day to debug and find the problem. the call-stack finally showed that the interrupt clears the TxState before it's set. ________________ Attachments : callstack-cdc-bug.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzNo&d=%2Fa%2F0X0000000bMZ%2FHLFltVnA6UMa4aXykip2lrJ_wGx8CHb2mgRUi61MzBA&asPdf=false2016-02-05 3:30 AM
Hi,
I confirm that the bug was fixed since the version 1.2.0 of STM32CubeL1 package (current one is 1.4.0).-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-04-03 11:46 PM
Hi Mayla,
I am currently using a STM32F072 with STM32CubeF0 1.4 and I am still having this problem.Mathieu2016-04-04 2:47 AM
Hi Mathieu,
The reported bug is already fixed since a while.This is the current implementation of USBD_CDC_TransmitPacket:uint8_t USBD_CDC_TransmitPacket(USBD_HandleTypeDef *pdev){ USBD_CDC_HandleTypeDef *hcdc = (USBD_CDC_HandleTypeDef*) pdev->pClassData; if(pdev->pClassData != NULL) { if(hcdc->TxState == 0) { /* Tx Transfer in progress */ hcdc->TxState = 1; /* Transmit next packet */ USBD_LL_Transmit(pdev, CDC_IN_EP, hcdc->TxBuffer, hcdc->TxLength); return USBD_OK; } else { return USBD_BUSY; } } else { return USBD_FAIL; }}It may be a different issue that you are facing. It should be better to clearly describe it.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-04-04 9:45 AM
Hi Mayla
first thank you for your quick answer. I do have this implementation of USBD_CDC_TransmitPacket in usb_dc.c. Yet, I still encounter this issue of TxState remaining equals to one, resulting in the microcontroller no longer writing. I use the USB communication in both directions, and this usually happens with dense traffic. I assume the situation where both the computer and the microcontroller can write at the same moment can happen. Would you have any recommandations regarding particular handshaking I would have to implement or things to avoid?Mathieu2016-04-05 10:20 AM
2016-04-10 9:37 PM
I'm working on an RNDIS device on STM32F429, using Cube HAL V1.9.
I'm using the same method as CDC to detect when the output frame has gone, and frequently getting the same problem as described here for CDC, with the flag being stuck on.I've done all of the patches described here, but hasn't helped at all. Anyone got any other suggestions on how to fix this issue?Not sure if I'm still facing ST's issue or if its something in my class driver code.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.