2019-02-20 7:24 AM
Hello All,
I need to read 4 ADC values with period of 1 Khz in interrupt mode.
After reading various post I found out that DMA will be used but I want to read multiple value periodically so should i use ADC injected conversion mode and set
No. of conversion to 4
External trigger source Timer 2 trigger out event
External trigger edge: Rising Edge
Injected Conversion mode to be discontinuous
Use Rank for various channels
I have a doubt that which to be used in main.c to start ADC i.e
HAL_ADC_START_DMA or HAL_ADC_START_IT
Also, is the approach use by me correct?
Regards,
Gunit
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.