2019-01-31 12:11 AM
I am working on STM32F779NI-EVAL board. I've tried the following QSPI example of stm32f769-eval board on STM32F779NI "..\en.stm32cubef7\STM32Cube_FW_F7_V1.14.0\Projects\STM32F769I_EVAL\Examples\QSPI\QSPI_ExecuteInPlace"
I'm facing an error in QSPI_WriteEnable(). HAL_QSPI_Command() call in the function times out.
However, with the same initialization sequence, the following example works perfectly on the same board.
"..\en.stm32cubef7\STM32Cube_FW_F7_V1.14.0\Projects\STM32F769I_EVAL\Examples\QSPI\QSPI_ReadWrite_DMA"
While debugging the issue, I found that status register for QSPI was not getting set as expected (QSPIHandle->Instance.SR).
Please share any pointers on the above issue. Thank you.
Solved! Go to Solution.
2019-02-06 4:35 AM
Hello,
Btw i tested on my side, both examples work properly.
Best Regards,
Mohamed Aymen.
2019-02-05 6:06 AM
Hello,
Can you please tell me the value of the status register ?
Best Regards,
Mohamed Aymen.
2019-02-06 4:35 AM
Hello,
Btw i tested on my side, both examples work properly.
Best Regards,
Mohamed Aymen.
2019-02-06 4:39 AM
Have you modified the board? Ie added any other boards or circuits, changed solder bridges or jumpers.
Do the external loaders in the ST-LINK Utilities or STM32 Cube Programmer work?
2019-02-06 5:11 AM
Hello,
It worked on my side too but the board is not getting reset using reset button on the board.Then I tried by unplugging and plugging the power adapter and it worked.
Can you tell me if it is working on your side @Mohamed Aymen HZAMI ??
Regards,
Akshay.
2019-02-06 8:14 AM
Hello,
Yes, it works perfectly.
Best Regards,
Mohamed Aymen.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.