2023-11-07 8:44 AM
Hi there,
I'm experimenting to develop my own bootloader on a NUCLEO-H755ZI-Q board using CubeIDE environment.
I prepared 2 "standard" projecs dedicated to the bootloader and to the application respectively.
On the Bootloader side, I redirected the printf output to the USART3 for debugging and it works fine.
Doing the same on the application side, printf is no longer working after jump from bootloader (no messages at all).
I already tried the HAL_UART_Transmit function and the peripheral seems work properly.
I already tried the HAL_UART_Transmit function and the peripheral seems work properly.
I verified syscall.c file is present... so what is missing?
Solved! Go to Solution.
2023-11-08 2:41 AM - edited 2023-11-08 2:44 AM
Hi @STea and @Tesla DeLorean ,
I tried overwriting _write function as suggested by @STea as follow in the main:
int _write(int file, char *ptr, int len)
{
HAL_UART_Transmit(&huart3, (uint8_t *) ptr, len, HAL_MAX_DELAY);
return len;
}
but no result!
Edit:
So,
I fixed the issue simply by adding "\r\n" at the endo of every message!
It seems that printf buffers strings and print them when it receive a new line sequence....
2023-11-07 8:59 AM
>> so what is missing?
Don't know, you'll have to debug, check clocks, RCC, that the baud rate relates to the bus/pll settings you have in effect.
Would suggest setting up all the MCU, AHB, APB clocks on the loader side, and then not change them on the app side.
2023-11-07 9:13 AM
Hello @iTTy ,
i suggest to make sure that the configuration of the clocks and uart3 instance is set correctly on the app side as recommended by @Tesla DeLorean . if it is the case i suggest you overload the __wirte function in syscall.c
int _write(int fd, char * ptr, int len)
{
HAL_UART_Transmit(&huart2, (uint8_t *) ptr, len, HAL_MAX_DELAY);
return len;
}
changing &huart2 to &huart3 .
hope this solves your request .
BR
Hichem
2023-11-08 2:41 AM - edited 2023-11-08 2:44 AM
Hi @STea and @Tesla DeLorean ,
I tried overwriting _write function as suggested by @STea as follow in the main:
int _write(int file, char *ptr, int len)
{
HAL_UART_Transmit(&huart3, (uint8_t *) ptr, len, HAL_MAX_DELAY);
return len;
}
but no result!
Edit:
So,
I fixed the issue simply by adding "\r\n" at the endo of every message!
It seems that printf buffers strings and print them when it receive a new line sequence....
2023-11-08 2:51 AM
Hello @iTTy
can you send me a copy of the main.c file so i can verify it with you again ?
also did you try to flush the uart buffer with fflush(0); after the printf call
exemple :printf("hello world");fflush(0);
BR
STea
2023-11-08 11:40 PM
Hi @STea ,
I attach the main file of the M7 project we are speaking about.
Environment context:
Mplab CubeIDE Version: 1.12.1 Build: 16088_20230420_1057 (UTC)
Standard (default) project created for a NUCLEO-H755ZI-Q with CubeMX version 6.5.0 with firmware package for STM32H7 version 1.10.0
Application context:
This is an application that will be launched by a bootloader (loader only work on M7 core without waking-up the M4 one; M7 loader jumps to the M7 application that release also the M4application).
I verified the issue: removing the "\r\n" sequence in the strings logged throughh the printf, nothing is sended to the terminal.
Regarding your last question: no, I don't tried fflush(0);....
Hope it is usefull!
iTTy
2023-11-09 5:39 AM
Hello @iTTy ,
adding fflush (0); resolves the problem also and printf on its own will work accordingly in run mode but when used in debug mode a fush off the UART buffer is needed here is the code example i have tried .
BR
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.