2025-10-06 3:03 AM - last edited on 2025-10-06 6:47 AM by Saket_Om
Board: STM32U5x9J-DK (Discovery)
MCU: STM32U5xx (U5G9J series)
STM32Cube package: STM32Cube_FW_U5_V1.8.0
Example path:
STM32Cube\Repository\STM32Cube_FW_U5_V1.8.0\Projects\STM32U5x9J-DK\Examples\OSPI\OSPI_NOR_MemoryMapped
File: main.c (write/read operations performed in switch(step), case 1)
IDE / toolchain: (please mention your IDE, e.g., STM32CubeIDE v1.19.0)
Running the example on the Discovery board: the write appears to run, memory-mapped mode is entered, but reading back returns garbage — the mismatch counter res always becomes 256 (I interpret that as every byte failed the compare). The write/read block is in case 1 of the main loop.
case 1:
if (CmdCplt != 0)
{
CmdCplt = 0;
/* ... set up mem-mapped write/read ... */
/* Writing Sequence ----------------------------------------------- */
mem_addr = (uint8_t *)(OCTOSPI1_BASE + address);
for (index = 0; index < BUFFERSIZE; index++)
{
*mem_addr = aTxBuffer[index];
mem_addr++;
}
HAL_Delay(MEMORY_PAGE_PROG_DELAY);
/* Reading Sequence ----------------------------------------------- */
mem_addr = (uint8_t *)(OCTOSPI1_BASE + address);
for (index = 0; index < BUFFERSIZE ; index++)
{
if (*mem_addr != aTxBuffer[index])
{
res++;
}
mem_addr++;
}
if (res != 0)
{ BSP_LED_On(LED_RED); }
else
{ BSP_LED_Toggle(LED_GREEN); HAL_Delay(50); }
/* ... */
}
break;
2025-10-10 3:39 AM
Hello @RC123,
The example works correctly. I recommend downloading the STM32Cube_FW_U5_V1.8.0 package again and following the instructions in the ReadMe file.
I hope my answer has helped you. When your question is answered, please select this topic as the solution that answered you, as it will help others find that answer faster.
Thanks for your contribution.
Dor_RH
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.