2026-02-17 9:32 PM - last edited on 2026-02-19 12:46 AM by mƎALLEm
I can build it successfully using west but when I program it I get: "Warning: The core is locked up" and no LED blinks.
I also made my own blinking LED but that doesn't work either.
I can program the board using stmcubeide and that work. It seems to be an stm32cubeprogrammer issue?
2026-02-18 5:31 AM
@curiousmind wrote:I also made my own blinking LED but that doesn't work either.
So what investigation/testing/debugging have you done to find why it's "not working" ?
How to write your question to maximize your chances to find a solution
2026-02-18 8:47 PM
I haven't gotten to debug it yet, I am new to Zephyr, I just wanted to try and run a simple application to begin with.
2026-02-19 8:20 PM
I managed to run the debugger, it goes to:
void z_arm_fault(uint32_t msp, uint32_t psp, uint32_t exc_return, _callee_saved_t *callee_regs)
{
uint32_t reason = K_ERR_CPU_EXCEPTION;
int fault = SCB->ICSR & SCB_ICSR_VECTACTIVE_Msk;
bool recoverable, nested_exc;
struct arch_esf *esf;with the fault 3.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.