2019-01-15 12:57 PM
In document DM00173145 Rev. 7 (STM32L4+ HAL and Low Layer Drivers) reference manual, there seems to be a section missing on the SD driver interface. There is a section SD Extension driver, but that doesn't have any of the general SD HAL API. Is this information available somewhere else ?
2019-01-23 4:30 AM
Hi @JVolp ,
You are right; the HAL SD Generic Driver section (that we find in UM1725, relative to STM32CubeF4 for example) is missing in UM1884 (Description of STM32L4/L4+ HAL and low-layer drivers).
A request is tracked internally to add it.
Meanwhile, you can refer to the chm files that you find under STM32Cube_FW_L4_V1.13.0\Drivers\STM32L4xx_HAL_Driver for a full description of SD APIs.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-03-11 1:42 AM
Hello @JVolp ,
Please note that the section "HAL SD Generic Driver" was added to the rev8 of UM1884, available on the web.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.