2025-02-25 1:54 AM - last edited on 2025-10-21 3:14 AM by Amel NASRI
Hello,
First of all, NetXDuo is working fine on the NUCLEO-H743ZI board. (PING, UDP, TCP)
Environment :
STM32CubeIDE v1.17.0
STM32CubeMX v6.13.0
STM32Cube_H7(HAL) v1.12.1
X-CUBE-AZRTOS-H7 v3.3.0
I modified it to fit my custom board.
The clock for the PHY chip is different.
It use by MCO1(25MHz) from MCU.
There is failed the _nx_driver_enable() function in nx_stm32_eth_driver.c file.
(PHYLinkState < ETH_PHY_STATUS_LINK_DOWN)
But, if the delay is reflected for more than 5 seconds before PHY initialization, normal operation is achieved.
(PING, UDP, TCP)
The same thing happens if I put a break point at that location in debug mode.
There is no PING response.
LwIP works fine on that board.
Best regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.