2020-09-14 9:08 AM
I believe there is a bug with the L496 series and the serial number the DFU firmware returns. Whenever I unpower and repower my board I get a different 12 digit hex number, for example this:
05FA03B042C5
becomes
F0F30783F95C
after next power cylce and so on. Anyone noticed this before? I couldn't find any note of this anywhere. Any suggestions for a work around?
I am writing a windows application to load a testing firmware through DFU, then do some testing and then load another app via DFU again and was planning on keeping track via this serial number. Alas, I cannot.
2020-09-15 1:18 AM
Can you try if a similar setup on some other type of CPU works reliable? That way we can excludes errors on your side.
2020-09-15 1:30 AM
Hi!
I have another device with the L452 which works fine. I actually wrote the whole programming system based on that device, and it worked fine. Then we switched to the L496 for more RAM and flash.
I don't even need to check it through my app. I open CubeProgrammer, switch to USB mode (DFU) and whenever I power cycle the L496 reports a different serial.
This is the board plugged in:
This is the same board when power cycled:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.