2020-07-27 9:04 AM
Hello!
I'm trying to interface a KSZ8081Phy with a STM32F767ZI MCU which is MII.
I was already able to interface with the RMII Phy o in the Nucleo-144 board.. So I replaced all the settings to able to run from an MII interface.
I'm running the Web Server demo include in the STM32CubeMX package. Now whenever I send a page load request from the PC, a packet is captures and it has the correct MAC address for the sender address . But the destination MAC address is always "0xff 0xff 0xff 0xff 0xff 0xff" which is a broadcast address.
The Web interface calls the netconn_accept which supposedly waits for a connection request. But that connection request is never actually received. I included the ethernetif.c file.
Any ideas how I can make this work?
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.