2025-03-26 5:30 AM - last edited on 2025-03-26 5:33 AM by mƎALLEm
I have jump function this like that but this method don't work. Please I need help immedietly
void jumpToAddress(uint32_t jump_address)
{
void (*jumpFunction)(void);
static constexpr uint32_t SHIFTED_JUMP_ADDRESS_DUE_TO_RESET_HANDLER = 4;
static constexpr uint8_t NVIC_REGISTER_LENGTH = 8;
SCB_DisableDCache();
SCB_DisableICache();
__disable_irq();
SysTick->CTRL = 0;
HAL_RCC_DeInit();
for (uint8_t i = 0; i < NVIC_REGISTER_LENGTH; i++)
{
NVIC->ICER[i] = 0xFFFFFFFF;
NVIC->ICPR[i] = 0xFFFFFFFF;
}
SCB->VTOR = jump_address;
__set_MSP(*((uint32_t *)jump_address + SHIFTED_JUMP_ADDRESS_DUE_TO_RESET_HANDLER));
jumpFunction = (void (*)(void))(*((uint32_t *)((jump_address + SHIFTED_JUMP_ADDRESS_DUE_TO_RESET_HANDLER))));
__enable_irq();
jumpFunction();
while (1);
}
2025-03-26 5:31 AM
Hello,
Please use </> button to share your code.
See the tips on this link. I'm editing your post.
Thank you for your understanding.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.