2020-04-08 10:15 PM
Using Firmware Package "STCubeFW_F4_V1.25.0" in CubeMX appears to cause various issues with generating code for USB HID mode. I was originally able to get a USB HID project working by following the USB HID Custom Device Lab tutorial (found here https://www.youtube.com/watch?v=3JGRt3BFYrM&t=325s) using firmware package 1.24.1 with the STM32F405. USB functionality was broken after migrating my project to V1.25.0, which causes my USB PC Host to report "Transfer error on interrupt endpoint: Operation timed out". In order to verify the problem was in fact part of the V1.25.0 package, I repeated the ST tutorial linked above with both versions of the firmware package and verified that the project is able to communicate with the HID_Terminal .exe application in V1.24.1 but crashes the application with the V1.25.0 version.
Some other issues I noticed using CubeMX include the following:
2022-08-19 7:48 AM
This seems to be a regression. I'm having the exact same issue on an STM32L073CBTx with Firmware Package STM32Cube FW_L0 V1.12.1. After adapting the generated code like in the youtube video: HID_terminal.exe works two times (sends and recieves data by clicking on Send-Button) but fails after the secound time with an error "Operation timed out".
The failure is reproducible on Linux with a similar app.
@ST: After one and a half year, please recreate the issue and fix it.
2022-08-19 10:11 AM
I've only tried this on the G4 so far, but here are a few things that got USB HID working after generating CubeMX code (some of this will be a repeat of information in the tutorial):
memcpy(g_usb_rx_bytes, state, 64);
USBD_CUSTOM_HID_SendReport(&hUsbDeviceFS, g_usb_tx_bytes, 64);
USBD_CUSTOM_HID_ReceivePacket(&hUsbDeviceFS);
return (USBD_OK);
2022-08-19 1:57 PM
USBD_CUSTOM_HID_ReceivePacket(&hUsbDeviceFS); <- this isn't in the tutorial, does that make the difference?
2022-08-19 2:02 PM
It did for me on the G4. I'm not sure if it will work for you but let me know if it does.
2022-08-19 2:16 PM
Looks a bit odd, but I'll test it tomorrow and get back to you. Thanks for your quick input!
2022-08-19 11:54 PM
In L0 there is no USBD_CUSTOM_HID_ReceivePacket(). Firmware Version V1.12.0 from year 2020 does work, ... so I guess I have to stick to that. But it would be nice if ST could fix the regression.
2022-08-20 3:19 PM
Open the file "stm32l0xx_hal_pcd.c" around line 1873 and change the if statement to the following:
/* Manage all non bulk transaction or Bulk Single Buffer Transaction */
if ((ep->type != EP_TYPE_BULK) ||
((ep->type == EP_TYPE_BULK) && ((wEPVal & USB_EP_KIND) == 0U)))
Let me know if that works.
2022-09-04 4:41 AM
--- a/Drivers/STM32L0xx_HAL_Driver/Src/stm32l0xx_hal_pcd.c
+++ b/Drivers/STM32L0xx_HAL_Driver/Src/stm32l0xx_hal_pcd.c
@@ -1851,28 +1851,6 @@ static HAL_StatusTypeDef PCD_EP_ISR_Handler(PCD_HandleTypeDef *hpcd)
/* clear int flag */
PCD_CLEAR_TX_EP_CTR(hpcd->Instance, epindex);
- if (ep->type != EP_TYPE_BULK)
- {
- ep->xfer_len = 0U;
-
- if ((wEPVal & USB_EP_DTOG_TX) != 0U)
- {
- PCD_SET_EP_DBUF0_CNT(hpcd->Instance, ep->num, ep->is_in, 0U);
- }
- else
- {
- PCD_SET_EP_DBUF1_CNT(hpcd->Instance, ep->num, ep->is_in, 0U);
- }
-
- /* TX COMPLETE */
-#if (USE_HAL_PCD_REGISTER_CALLBACKS == 1U)
- hpcd->DataInStageCallback(hpcd, ep->num);
-#else
- HAL_PCD_DataInStageCallback(hpcd, ep->num);
-#endif /* USE_HAL_PCD_REGISTER_CALLBACKS */
- }
- else
- /* Manage Bulk Single Buffer Transaction */
if ((ep->type != EP_TYPE_BULK) ||
((ep->type == EP_TYPE_BULK) && ((wEPVal & USB_EP_KIND) == 0U)))
{I had to apply the above patch to get it working - but I have 0 idea why it does! - an answer from ST would be great.
2022-09-04 1:15 PM
the ST code seems obviously wrong: They double test for ep->type != EP_TYPE_BULK:
if (a) {
...
} else if (a || b) {
...
}... @ST: any comment???
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.