2019-06-06 10:46 AM
Hello,
I'm using VCP to communicate with an STM32F303 device, which works well.
However, when I plug a second device on the same computer, it fails to enumerate properly with the message 'This device cannot start. (Code 10)'.
Is that a known issue?
Is there a way to connect several STM32 on the same computer?
Thanks
jyl
2019-06-06 11:11 AM
And if you unplug the first device and plug in the second one?
Don't they draw excessive power?
JW
2019-06-06 1:37 PM
Non unique "serial number" ?
-- pa
2019-06-06 3:30 PM
Hmm, maybe same ID...
I thought serial number was assigned automatically for each device...
I'll check this in mode details.
Thanks Pavel!
2019-06-06 3:32 PM
Both work perfectly as long as they are alone on the computer...
jyl
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.